Skip to main content
aaron
Associate II
March 12, 2014
Question

Application note for LPS25H?

  • March 12, 2014
  • 4 replies
  • 1327 views
Posted on March 13, 2014 at 00:22

I am interested in the LPS25H MEMS barometer chip, but I am having a hard time figuring out the footprint of the HCLGA-10L package.

Here is what is called out in the datasheet:

0690X00000605TMQAY.png

I cannot decipher from his what the dimensions of the pads should be.  I believe that e1/2 might give me the width, but I cannot determine the length.  Maybe that's what B is supposed to mean, but I don't see it.

Also, I found that there is a

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00064026.pdf

but cannot find one for the LPS25H.  I realize it's a very new part, but this would help -- it provides some guidance on how the pads should be laid out.

Can someone more mechanically inclined parse this for me?

Thanks.

#hclga-10l

4 replies

aaron
aaronAuthor
Associate II
March 15, 2014
Posted on March 15, 2014 at 14:28

For reference, here is the figure of merit from the LPS331AP, which is a comparable part (though with worse resolution).

0690X00000605TRQAY.png

T1 and T2 give the dimensions of the pads, and the rest can be inferred easily.

I suppose I should just use the LPS331AP instead...

gh_it
Associate
August 8, 2014
Posted on August 08, 2014 at 11:33

Getting support for ST is much harder than getting blood out of a stone.  They are at Rev 3 of this data sheet and still haven't dealt with this problem.

Freescale make a couple of nice parts which are similar in price.

Nickname3460_O
Visitor II
October 2, 2014
Posted on October 02, 2014 at 07:10

Hello,

Infact we are going to improve the quality of the drawing with more details;

The pad dimension you are looking for are: 0.30mm x 0.45mm (+/- 0.05 mm tolerance)

You can find the LPS25H AN just below the LPS331AP , at this address

http://www.st.com/stonline/stappl/resourceSelector/app?page=fullResourceSelector&doctype=application_note&SubClassID=1316

Thank you for your questions

Visitor II
December 23, 2024

Please update the entire datasheet while you're at it. The "Application hints" page is very hard to read like this, a footprint is not a schematic... And Table 2 could use an update as well like input/output/open collector info etc. And I'd expect some information on how long a measurement takes, min/typ/max etc.