Skip to main content
leewonsoo
Associate
April 23, 2018
Question

Interrupt that will not expected

  • April 23, 2018
  • 2 replies
  • 1574 views
Posted on April 23, 2018 at 03:59

Hello,

- MCU : STM8L101K3

I am using Port A.2 for interrupt and Port D.2 for general gpio.

GPIO_Init(GPIOA,GPIO_Pin_2, GPIO_Mode_In_FL_IT);

EXTI_SetPinSensitivity(EXTI_Pin_2, EXTI_Trigger_Falling);

GPIO_Init(GPIOD, GPIO_Pin_2, GPIO_Mode_Out_PP_High_Fast);

In my scenario, Port D.2 is changed input to output mode per every 1sec.

if(onesec)

{

   onesec = 0;

   GPIO_Init(GPIOD, GPIO_Pin_2, GPIO_Mode_In_FL_No_IT); // all led off

   if(redled)

   {

      GPIO_Init(GPIOD, GPIO_Pin_2, GPIO_Mode_Out_PP_High_Fast);

      GPIO_ResetBits(GPIOD, GPIO_Pin_2); // red led on

   }

   else if(blueled)

   {

      GPIO_Init(GPIOD, GPIO_Pin_2, GPIO_Mode_Out_PP_High_Fast);

      GPIO_SetBits(GPIOD, GPIO_Pin_2); // blue led on

   }

   else //led off

   {

      // nothing.

   }

}

If this condition is redled, The EXTI2_IRQHandler that will not expected is called.

0690X0000060AjPQAU.png

The Port A.2's hardware line is not interrupted in oscillscope.

Please know me why 

EXTI2_IRQHandler is called?

Thanks in advance.

    This topic has been closed for replies.

    2 replies

    Szymon PANECKI
    Senior III
    April 23, 2018
    Posted on April 23, 2018 at 11:03

    Hello,

    EXTI controller is designed is a way, that EXTI[number] is connected to all Px[number] pins. This means that EXTI2 IRQ handler will react on signal change on very pin, which has 2 in the name: PA2, PB2, PC2 andPD2. Pleas see below the extract from MCU's reference manual.

    0690X0000060AjKQAU.png

    I believe that this could be an explanation of the bahavior, that you faced.

    Regards

    Szymon

    leewonsoo
    leewonsooAuthor
    Associate
    April 23, 2018
    Posted on April 23, 2018 at 11:37

     ,

     ,

    Thanks.

    I have one more question.

    In output mode, level change is not affects to same interrupt's pin ♯ .

    What is the exact meaning of the signal change? ,

    Regards

    leewonsoo