Skip to main content
armindavatgaran
Associate III
January 2, 2015
Question

System clock configuring with stm32cube

  • January 2, 2015
  • 1 reply
  • 497 views
Posted on January 02, 2015 at 11:44

Hello

I have 2 questions :

1 - According to this library and sample examples , HAL_Init() function is called at the start of the main() that configures the systemtick timer for generating 1ms interrupts , but after that the SystemClock_Config() is called which configures the plls and other clock related parameters for increasing core clock to 168 MHz(for example for stm32f4) .

But by this work , the systick timer will not make precesion interrupts anymore because its time base has changed without any updating .

2 - According to page 368 of RM0090 , SysTick has fixed calibration value with HCLK set to 150 MHz but we have 168 MHz in stm32f4 , So its time base is not 1 ms and can not be changed, is it right ?

Please help, thanks .
    This topic has been closed for replies.

    1 reply

    armindavatgaran
    Associate III
    February 28, 2015
    Posted on February 28, 2015 at 18:26

    Anyone to answer?