Skip to main content
FaintSmile
Associate
February 7, 2015
Question

Keil - Failed to reset CPU -

  • February 7, 2015
  • 1 reply
  • 1217 views
Posted on February 07, 2015 at 11:43

Hi,

I have made my own pcb design using STM32F407VGT6 in LQFP100 package.I used the stm32f4 launch board schematic.I pulled down the boot0  and boot1 pins using voltage divider (10k//510).I connected 15  100nf caps to vdd pins and 2.2 uF caps  to Vcap pins , 100nf cap  to nrst pin also used ld1117 3.3 v regulator with 22uF output capacitor.

At first pcb worked fine and  I downloaded my code to flash using j-link edu.But after I pressed the reset button  MCU failed to start-up so i tried to download my code again and i got this error log from keil.

* JLink Info: Found SWD-DP with ID 0x2BA01477

* JLink Info: Found SWD-DP with ID 0x2BA01477

* JLink Info: Found Cortex-M4 r0p1, Little endian.

* JLink Info: FPUnit: 6 code (BP) slots and 2 literal slots

* JLink Info: TPIU fitted.

* JLink Info: ETM fitted.

ROMTableAddr = 0xE00FF003

* JLink Info: SYSRESETREQ has confused core. Trying to reconnect and use VECTRESET.

* JLink Info: Found SWD-DP with ID 0x2BA01477

**JLink Warning: Failed to reset CPU. VECTRESET has confused core.

**JLink Warning: CPU did not halt after reset.

**JLink Warning: CPU could not be halted

* JLink Info: Core did not halt after reset, trying to disable WDT.

**JLink Warning: CPU did not halt after reset.

**JLink Warning: CPU could not be halted

**JLink Warning: Could not set S_RESET_ST

* JLink Info: Found SWD-DP with ID 0x2BA01477

* JLink Info: SYSRESETREQ has confused core. Trying to reconnect and use VECTRESET.

* JLink Info: Found SWD-DP with ID 0x2BA01477

**JLink Warning: Failed to reset CPU. VECTRESET has confused core.

**JLink Warning: CPU did not halt after reset.

**JLink Warning: CPU could not be halted

* JLink Info: Core did not halt after reset, trying to disable WDT.

**JLink Warning: CPU did not halt after reset.

**JLink Warning: CPU could not be halted

**JLink Warning: Could not set S_RESET_ST

***JLink Error: Error while identifying Cortex-M core.

**JLink Warning: CPU could not be halted

It seemed like j link can not reset the MCU so I tried to reset the MCU with  pulling down the  nrst pin with jumper and tried again but that did not work at all.Should I use a bigger capacitor or connect 1k resistor to nrst pin as shown in olimex pcb design.

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    February 7, 2015
    Posted on February 07, 2015 at 12:51

    If the code you downloaded is broken, it may disconnect JTAG/SWD connectivity.

    Suggest you repeat your experiment with BOOT0 strapped HIGH

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..