STM32F103 option byte PGERR
Posted on December 27, 2016 at 14:31
I'm trying to write the option bytes, but I get PGERR or Imprecise data bus error.
Here is some psuedo code that is what is happening. The HAL also does this, that's why I started from scratch using the programming manual. But to no avail.
... HSI is ON. Prefetch if off... two wait states
_FLASH_CR_unlock();
__disable_irq();
FLASH->OPTKEYR = FLASH_KEY1;
FLASH->OPTKEYR = FLASH_KEY2;
FLASH->CR |= FLASH_CR_OPTPG;
FLASH->SR |= FLASH_SR_EOP | FLASH_SR_WRPRTERR | FLASH_SR_PGERR;
*0x1FFFF804 = 0xAA;
while(FLASH->SR & FLASH_SR_BSY);
// Check for EOP bit and compare data.
uint32_t SR = FLASH->SR;
... check and return flags
I've asked this before, in the old forum. However, I need this, so I'll ask again.