Skip to main content
ionutF
Associate III
February 17, 2016
Question

STM MCU with embedded 485

  • February 17, 2016
  • 2 replies
  • 1002 views
Posted on February 17, 2016 at 15:48

Is there a STM MCU with RS-485 integrated on it ? It would be very usefull  given the fact that MCUs are industriall devices and one of the most used communication protocol in industry is RS-485.   

    This topic has been closed for replies.

    2 replies

    Nesrine M_O
    Associate
    February 17, 2016
    Posted on February 17, 2016 at 16:58

    Hi ionut.fasola,

    RS485 Driver Enable is a hardware feature implemented in USART for 

    F0/F3/F7/L4/L0 products.

    -Syrine-

    Tesla DeLorean
    Guru
    February 17, 2016
    Posted on February 17, 2016 at 18:28

    Having the driver circuitry on chip isn't really appropriate for a general purpose micro-controller. If you want CAN, RS232 or RS485 you need to integrate the appropriate off-the-shelf driver chips into your design.

    The drivers likely use wholly different processes and geometries.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..