Skip to main content
tome
Associate II
October 13, 2017
Question

STM32F103 MDK-ARM5 NVIC can't change an address.

  • October 13, 2017
  • 7 replies
  • 2588 views
Posted on October 13, 2017 at 12:55

Hello comunity,

I trying to write a bootloader that will copy firmware from one memory range to other. And I need your help with understanding what is going on with my STM32F106C8T6 and what I doing wrong.

Incoming data:

-bootloader      0x08000 0000

-KEY                0x08000 4c00

-FW_main       0x08000 5000

-FW_Source   0x08000 A000

i'ts start addreses for each part of my program.

Logic of program:

Bootloader starts and chek is the KEY-dada exist on the KEY addres.

Here two ways:

- If KEY-data exist - bootloader starts copying data from FW_Source memory range to FW_main memory range. After copying all FW_Source data, we clean KEY-data,  FW_Source-data and reboot. 

-If KEY-data data other way it jumps to the address FW_main + 4.

On this stage all what we should to know. 

Im using Keil MKD ARM 5 with HAL. When I want writing firmware to the address 0x08000 A000 I shoud to edit ProjectName.stc file

---

; *************************************************************

; *** Scatter-Loading Description File generated by uVision ***

; *************************************************************

LR_IROM1 0x0800A000 0x00010000 { ; load region size_region

ER_IROM1 0x0800A000 0x00010000 { ; load address = execution address

*.o (RESET, +First)

*(InRoot$$Sections)

.ANY (+RO)

}

RW_IRAM1 0x20000000 0x00005000 { ; RW data

.ANY (+RW +ZI)

}

}

---

Then I could to flush stm32f103 in the right memory ranege. I check it end everything is ok.

If after copying data from 

FW_Source   to 

FW_main  I 

didn't erase the

FW_Source 

memory rage. The aplication works as i expexted it's jump to the

0x080005000 and works fine. 

But! If I ereasing 

FW_Source  range it's stop worknig. 

So, as I understand I need to move NVIC table to the new address (0x08005000), as HAL don't have a function 

NVIC_SetVectorTable I deside to write it directly to the register SCB->VTOR = 0x08005000;  But, this didn't help me.

--- User aplication code ---

int main(void)

{

/* USER CODE BEGIN 1 */

__set_PRIMASK(1);

SCB->VTOR = 0x08005000;

//__set_MSP(*(__IO uint32_t*) 0x08005000); //-- ???? ?? ?????

__set_PRIMASK(0);

/* USER CODE END 1 */

...

---

Then, I tryed to comment data in the systeminit() (

system_stm32f1xx.c).But this also didn't help me.

---

&sharpifdef VECT_TAB_SRAM

SCB->VTOR = SRAM_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal SRAM. */

&sharpelse

//SCB->VTOR = FLASH_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH. */

&sharpendif

--- 

Also I tryed set the SCB->VTOR in the bootloader jumb function, but and this didn't help.

---

void jumpToApplication(uint32_t addr)

{

typedef void (*pFunction)(void);

pFunction Jump_To_Application;

uint32_t JumpAddress;

JumpAddress = *(__IO uint32_t*) (addr + 4);

Jump_To_Application = (pFunction) JumpAddress;

SCB->VTOR = addr; //set NVIC table

__set_MSP(*(__IO uint32_t*) addr);

Jump_To_Application();

}

---

I'm confused, while reading manuals I didn't finde anything that can explain why it's didn't work. So, community I need your help .

Best regards,

Sergii Kirichok 

#nvic #mdk-armv5 #stm32f1 #stm32 #bootloader
This topic has been closed for replies.

7 replies

Tesla DeLorean
Guru
October 13, 2017
Posted on October 13, 2017 at 13:22

You need to build the code for the address you expect to run it at and not the address you park it at before copying.

The vector table contains absolute addresses. 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
tome
tomeAuthor
Associate II
October 13, 2017
Posted on October 13, 2017 at 15:08

Thank you for your answer.

You are right, I if build frimware with configured someproject.stc to the  0x08005000 adreses It works, I knew it before. But, while I testing (copying firmware from one segment to other) , I nedded to to flush it to one andress and run from other. I can't understand, what could to do liker, that can't be changed from the aplicaton.

Tesla DeLorean
Guru
October 13, 2017
Posted on October 13, 2017 at 15:39

Addresses described *IN* the Vector Table, not the tables address. 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..