Skip to main content
sanjib
Associate III
May 27, 2014
Question

I2c on stm32f030r8t6

  • May 27, 2014
  • 7 replies
  • 1206 views
Posted on May 27, 2014 at 09:03

Before posting here I have gone through stm32f0_stdperiph_lib.zip but the examples which are given are for some different board with different architecture. can anyboduy point me a simple example of communication between two stm32f030r8t6 boards , one will be master and it will be received data from the slave in an way of interrupt not polling. Please help me

    This topic has been closed for replies.

    7 replies

    sanjib
    sanjibAuthor
    Associate III
    May 27, 2014
    Posted on May 27, 2014 at 14:27

    Hi can anybody help me

    Tesla DeLorean
    Guru
    May 27, 2014
    Posted on May 27, 2014 at 17:22

    Hi can anybody help me

    The forum seems to be saying no.

    The STM32F0xx_StdPeriph_Lib_V1.3.1\Projects\STM32F0xx_StdPeriph_Examples\I2C\I2C_TwoBoards\readme.txt

    is for the EVAL series boards, what prevents you from porting this? Does the F03 I2C bus work differently?
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    sanjib
    sanjibAuthor
    Associate III
    May 28, 2014
    Posted on May 28, 2014 at 06:31

    I dont have LCD in my board and the API's used in this project are not present in my board

    stm32f030r8t6
    sanjib
    sanjibAuthor
    Associate III
    May 28, 2014
    Posted on May 28, 2014 at 13:55

    I have used the fr07 i2c code for reference and writing the fo3o code......but api's like I2C_CheckEvent(I2Cx, I2C_EVENT_MASTER_MODE_SELECT))&&(TimeOut != 0x00))

    and others are not in stm32f030 how shud I do that I am attaching my code

    ________________

    Attachments :

    I2c.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzzp&d=%2Fa%2F0X0000000bRv%2FgNfi._EVa.ygdrKbxBgXeUdBiRg_cgTREl.KzzVqaDg&asPdf=false
    sanjib
    sanjibAuthor
    Associate III
    May 28, 2014
    Posted on May 28, 2014 at 15:16

    now im trying in this way.. but something its wrong.. on a terminal im getting only ''error2''.. any ideas? ;)
    
    
     #include ''stm32f0xx.h''
    #include ''stm32f0xx_rcc.h''
    #include ''stm32f0xx_gpio.h''
    #include ''stm32f0xx_usart.h''
    #include ''stm32f0xx_i2c.h''
    #include <
    stdio.h
    >
    GPIO_InitTypeDef GPIO_InitStructure;
    USART_InitTypeDef USART_InitStructure;
    I2C_InitTypeDef I2C_InitStructure;
    #define MPU6050_RA_WHO_AM_I 0x75
    #define Slave_address 0x68
    #define mpu6050_FLAG_TIMEOUT ((uint32_t)0x1000)
    #define mpu6050_LONG_TIMEOUT ((uint32_t)(500 * mpu6050_FLAG_TIMEOUT))
    void USART_send( unsigned char data){
    while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET);
    USART_SendData(USART1, data);
    }
    void USART_print(char* StringPtr){
    while(*StringPtr != 0x00){
    USART_send(*StringPtr);
    StringPtr++;}
    }
    void frej(uint8_t value)
    {
    int maska=0x01;
    int i;
    for(i=7;i>=0;i--){
    int l = (((int)value)>>i)&maska;
    char t = (char)(l+48);
    USART_send(t);
    }
    USART_send(' ');
    }
    uint8_t ReadReg(uint8_t RegName)
    {
    uint8_t mpu6050_BufferRX[2] ={0,0};
    uint8_t tmp = 0;
    uint32_t DataNum = 0;
    int mpu6050_Timeout = 0;
    /* Test on BUSY Flag */
    mpu6050_Timeout = mpu6050_LONG_TIMEOUT;
    while(I2C_GetFlagStatus(I2C1, I2C_ISR_BUSY) != RESET)
    {
    if((mpu6050_Timeout--) == 0) USART_print('' error1 '');
    }
    /* Configure slave address, nbytes, reload, end mode and start or stop generation */
    I2C_TransferHandling(I2C1, Slave_address, 1, I2C_SoftEnd_Mode, I2C_Generate_Start_Write);
    /* Wait until TXIS flag is set */
    mpu6050_Timeout = mpu6050_LONG_TIMEOUT;
    while(I2C_GetFlagStatus(I2C1, I2C_ISR_TXIS) == RESET)
    {
    if((mpu6050_Timeout--) == 0) USART_print('' error2 '');
    }
    /* Send Register address */
    I2C_SendData(I2C1, (uint8_t)RegName);
    /* Wait until TC flag is set */
    mpu6050_Timeout = mpu6050_LONG_TIMEOUT;
    while(I2C_GetFlagStatus(I2C1, I2C_ISR_TC) == RESET)
    {
    if((mpu6050_Timeout--) == 0) USART_print('' error3 '');
    }
    /* Configure slave address, nbytes, reload, end mode and start or stop generation */
    I2C_TransferHandling(I2C1, Slave_address, 1, I2C_AutoEnd_Mode, I2C_Generate_Start_Read);
    /* Reset local variable */
    DataNum = 0;
    /* Wait until all data are received */
    while (DataNum != 1)
    {
    /* Wait until RXNE flag is set */
    mpu6050_Timeout = mpu6050_LONG_TIMEOUT;
    while(I2C_GetFlagStatus(I2C1, I2C_ISR_RXNE) == RESET)
    {
    if((mpu6050_Timeout--) == 0) USART_print('' error4 '');
    }
    /* Read data from RXDR */
    mpu6050_BufferRX[DataNum]= I2C_ReceiveData(I2C1);
    /* Update number of received data */
    DataNum++;
    }
    /* Wait until STOPF flag is set */
    mpu6050_Timeout = mpu6050_LONG_TIMEOUT;
    while(I2C_GetFlagStatus(I2C1, I2C_ISR_STOPF) == RESET)
    {
    if((mpu6050_Timeout--) == 0) USART_print('' error5 '');
    }
    /* Clear STOPF flag */
    I2C_ClearFlag(I2C1, I2C_ICR_STOPCF);
    // !< Store LM75_I2C received data
    //tmp = (uint16_t)(LM75_BufferRX[0] << 8);
    //tmp |= LM75_BufferRX[0];
    tmp = mpu6050_BufferRX[0];
    // return a Reg value
    return (uint8_t)tmp;
    }
    void LED_init(void){
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9|GPIO_Pin_8;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
    GPIO_Init(GPIOC, &GPIO_InitStructure);
    }
    void USART_init(void){
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1,ENABLE);
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1);
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1);
    //Configure pins: Rx and Tx --------------------------
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    USART_InitStructure.USART_BaudRate = 9600;
    USART_InitStructure.USART_WordLength = USART_WordLength_8b;
    USART_InitStructure.USART_StopBits = USART_StopBits_1;
    USART_InitStructure.USART_Parity = USART_Parity_No;
    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
    USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
    USART_Init(USART1, &USART_InitStructure);
    USART_Cmd(USART1,ENABLE);
    }
    void I2C_init(void){
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE);
    /* Configure the I2C clock source. The clock is derived from the HSI */
    RCC_I2CCLKConfig(RCC_I2C1CLK_HSI);
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_1);
    GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_1);
    //Configure pins: SCL and SDA ------------------
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;
    GPIO_Init(GPIOB, &GPIO_InitStructure);
    I2C_InitStructure.I2C_AnalogFilter = I2C_AnalogFilter_Enable;
    I2C_InitStructure.I2C_DigitalFilter = 0x00;
    I2C_InitStructure.I2C_OwnAddress1 = 0x00; // MPU6050 7-bit adress = 0x68, 8-bit adress = 0xD0;
    I2C_InitStructure.I2C_Mode = I2C_Mode_I2C;
    I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;
    //I2C_InitStructure.I2C_Timing = 0xA0120227;
    I2C_InitStructure.I2C_Timing = 0x20310A0D;
    I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;
    I2C_Init(I2C1, &I2C_InitStructure);
    I2C_Cmd(I2C1, ENABLE);
    }
    int main(void)
    {
    LED_init();
    USART_init();
    I2C_init();
    int i=0;
    while(1)
    {
    while (USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); // Wait for Empty
    ReadReg(MPU6050_RA_WHO_AM_I);
    for(i=0;i<10000000;i++);
    /*
    int i=0;
    if(USART_ReceiveData(USART1)=='x'){
    GPIO_SetBits(GPIOC, GPIO_Pin_8);
    }
    for(i=0;i<1000000;i++);
    GPIO_ResetBits(GPIOC, GPIO_Pin_8);
    for(i=0;i<1000000;i++);
    */
    }
    }

    sanjib
    sanjibAuthor
    Associate III
    May 29, 2014
    Posted on May 29, 2014 at 07:22

    any body can give me idea

    sanjib
    sanjibAuthor
    Associate III
    May 29, 2014
    Posted on May 29, 2014 at 12:05

    OK,I found the problem. Flag I2C_ISR_TXIS did not get because the device on the i2c did not respond to the sent address. Need to convert the device address to 7 bits.