Associate
March 29, 2014
Question
STM32F4 Discovery no I/O toggle
- March 29, 2014
- 6 replies
- 1893 views
Posted on March 29, 2014 at 19:51
I am trying to toggle an I/O line to measure timing for benchmarking dsp algorithms on an STM32F407VGT. I generated the HAL using STM32CubeMX and set PD12 and PC8 to outputs and configured them as output push-pull with no pull-up. The generated code includes the following which is called prior to entering the infinite while in main().
/*Configure GPIO pin : PD12 */GPIO_InitStruct.Pin = GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_MEDIUM;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);Later I use the following to set and reset the I/O pin: // Set PD12 at the beginning of the calculation
HAL_GPIO_WritePin(GPIOD, 12, GPIO_PIN_SET);
// Clear PD12 at the end of the calculation
HAL_GPIO_WritePin(GPIOD, 12, GPIO_PIN_RESET);Yet, the I/O pin is not toggling. I believe I configured the clock tree correctly and I'll include a screen grab from STM32CubeMX. Am I missing anything obvious? Thanks!