STM32cube Version 4.20.0 bugs
Hello,
ST, please, do not release untested versions of STM32CubeMX, because we used to trust this software. And now it is just one big BUG... I have updated Cube, because wanted to set STM32F7 hardware JPEG encoder, but other parts just does not work as expected... Lets say I can understand, that newer Cube version 'does not like' older Firmware packages (tried to compile Cube generated code with STM32Cube_FW_F7_V1.4.0, but got 20 errors with missing structures and so on), but I can not understand when functions are missing with newest package (
STM32Cube_FW_F7_V1.6.0)...
All these bugs appears when I select STM32F746NGHx STM32F746G-DISCO board.
Find two differences:
// new code
void MX_SDMMC1_SD_Init(void)
{hsd1.Instance = SDMMC1;
hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING; hsd1.Init.ClockBypass = SDMMC_CLOCK_BYPASS_DISABLE; hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE; hsd1.Init.BusWide = SDMMC_BUS_WIDE_1B; hsd1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE; hsd1.Init.ClockDiv = 0;}
// and older code
void MX_SDMMC1_MMC_Init(void)
{hmmc1.Instance = SDMMC1;
hmmc1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING; hmmc1.Init.ClockBypass = SDMMC_CLOCK_BYPASS_DISABLE; hmmc1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE; hmmc1.Init.BusWide = SDMMC_BUS_WIDE_1B; hmmc1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_ENABLE; hmmc1.Init.ClockDiv = 0; if (HAL_MMC_Init(&hmmc1) != HAL_OK) { Error_Handler(); }HAL_MMC_ConfigWideBusOperation(&hmmc1, SDMMC_BUS_WIDE_8B);
}
There are many more bugs, but they are not so much annoying: examples have different structure from cube generated projects, a lot of examples does not work with/without optimizations and so on and on, there would not be end...
Thank You.