Skip to main content
vincenthamp9
Associate III
July 21, 2015
Question

IIR biquad testing - float64 MATLAB vs. CMSIS [solved]

  • July 21, 2015
  • 0 replies
  • 739 views
Posted on July 21, 2015 at 15:43

Hello there

I've been trying to implement an IIR biquad lowpass filter with the DSP library lately. I started out by designing the filter in MATLAB and calculating the IIR parameters before I pretty much copied the code from ARMs CMSIS page. The low pass should filter a 320 double long input signal stored in ''testInput_f64''. The filter itself should also be double precision, so I used the df2T float64 version of the IIRs.

float64_t testInput_f64[320] = { * here are 320 doubles ... * };
float64_t testOutput_f64[320] = {0};
const float64_t coeffs[5] = { 0.0168191501070571,
0.0336383002141143,
0.0168191501070571,
-1.60109239418362,
0.668368994611848};
static float64_t biquadStateBandF64[4]; // one stage -> 4x state variables {x[n-1], x[n-2], y[n-1], y[n-2]}

 int main(void)
 {
 arm_biquad_cascade_df2T_instance_f64 S1;
 float64_t *inputF64, *outputF64;

 /* Link */
 inputF64 = &testInput_f64[0];
 outputF64 = &testOutput_f64[0];

 /* Initialize biquad f64 */
 arm_biquad_cascade_df2T_init_f64 (&S1, 1, (float64_t *) &coeffs[0], &biquadStateBandF64[0]);
 /* Run biquad */
 arm_biquad_cascade_df2T_f64(&S1, inputF64, outputF64, 320);
 } 

Although the code compiles and runs fine the results aren't really satisfying. The first two results come somewhat close to what I get in MATLAB, but everything else is plain wrong. How could that be? I chose the double precision for a reason, since I though its almost 1:1 compareable to what MATLAB would calculate... Am I missing something here? Thanks /edit For future reference... MATLABs denominator is negated, compared to the definition used in the DSP lib.
    This topic has been closed for replies.