Skip to main content
giovanni2
Associate II
June 16, 2014
Question

RTC subseconds issue

  • June 16, 2014
  • 1 reply
  • 602 views
Posted on June 16, 2014 at 15:25

Hi,

I am working on STM32F303VCT6.

The source clock is a cristal of 32.768Khz.

I need to have a time resolution on the RTC of 1ms. So I have arranged the prescalers as follow:

SynchPrediv = 0x3E7; 

 AsynchPrediv = 0x21;

My idea is to have a frequency on the second counter (Synchronous prescaler) of about 1khz. Doing this I should have the possibility to have a value on the RTC_SS register from 0 to 999, that means 1ms for each steps.

the time in msec = (Prediv_Sync - SS)/(Prediv_Sync + 1) (Ref. Manual pag.643)

If I put a function GetSubseconds() inside an external interrupt routine ( external pin ) that is connected to an external source ( 100hz) I should have a difference of the two value read by the function GetSubseconds() of about 10. Am I right?

( I am sure that the time intervall between the two consequenzial GetSubseconds() function call is really 10ms, because I have put a logic toggle on a pin and show it on my oscilloscope)

Instead I read about 3, 4 steps...

The RTC works fine, If I try to read the time each 1sec, the time is correct, 1sec of increment...

I don't understand
    This topic has been closed for replies.

    1 reply

    giovanni2
    giovanni2Author
    Associate II
    June 16, 2014
    Posted on June 16, 2014 at 16:01

    Solved!!

    RTC registers were not updated correctly

    thk