Skip to main content
B.Michele
Associate III
November 10, 2015
Question

Power Voltage Detector(PVD) and PA0-WKUP PIn of STM32F100

  • November 10, 2015
  • 0 replies
  • 486 views
Posted on November 10, 2015 at 14:54

Good morning,  Someone have try to enable the PVD function, and use

the PA0-WKUP  Pin like an Output ??  When i start the PVD functions 

although i disable the Wake Up pin  (PWR_WakeUpPinCmd (DISABLE);)

I am not able to control the PA0 like an Output ?? Not function more....

If i disable the PVD the Output PA0 function, normally!, there is some configuration  

 to do ??

thank you
    This topic has been closed for replies.