2014-05-21 12:43 PM
i am using STM32f207
i have a flash memory connected to SPI2. I used the ST examples and i got it working, read/write, .. great, ... the problem is the speed ... how fast can i run SPI2? There is a setting SPI_InitStruct.SPI_BaudRatePrescaler and the lowest value is SPI_BaudRatePrescaler_2In my SetSysClock function i set the dividers to 1: http://prntscr.com/3lbcy6This should give me the fastest speed?My flash goes up to 85MHz and i need to go at least 80MHz because there is a lot of data to read in short time .. will this be possible on SPI2? I have a 25MHz xtal on the board and i am running the ST at 120MHz via PLL.2014-05-21 12:49 PM
maybe if i want to go that fast i need use I/O?
2014-05-21 12:55 PM
In my SetSysClock function i set the dividers to 1: This should give me the fastest speed?
Wouldn't it just break the buses? APB1 has a max of 30 MHz, APB2 60 MHz For faster flash interfacing consider SDIO2014-05-21 1:24 PM
i see .. i saw that in the ref manual but i did not want to believe it .. ok i will use i/o then .. thank you
2014-05-21 1:27 PM
can i connect SPI2 to AHB2?
2014-05-21 1:32 PM
about breaking the busses, HCLK is the xtal freq right? so 25mhz will not break ahb1 if i set the ahb1 divider to 1?
2014-05-21 2:11 PM
can i connect SPI2 to AHB2?
I'm not sure how you plan on achieving that without reworking the silicon.about breaking the busses, HCLK is the xtal freq right? so 25mhz will not break ahb1 if i set the ahb1 divider to 1? No, it's the CPU (PLL) clock at 120 MHz, or a fraction thereof (1 .. 512). Review the clock tree You could bit bang the part, as you suggest, there are other 4-bit (quad) SPI Flash devices too
2014-05-21 2:17 PM
2014-05-22 12:04 AM
From the DataSheet ...
''The STM32F20x devices feature up to three SPIs in slave and master modes in full-duplex and simplex communication modes. SPI1 can communicate at up to 30 Mbits/s, while SPI2 and SPI3 can communicate at up to 15 Mbit/s.'' Thus, even using all three channels simultaneously, the SPI hardware does not support the required throughput.2014-05-27 5:15 PM
Thank you i setup the clocks correctly now .. switched to SPI1 and all is good now thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.