Problem with stm32f4 discovery & stm32-mat/target
- May 6, 2014
- 7 replies
- 2378 views
Hi,
I am trying to get my stm32f4 discovery working with the Matlab/Simulink package provided by ST.
I am using Matlab R2014a V8.3on Windows 7. I am using Keil µVision 4.72 as toolchain. When I am trying theBlinkBlueLed
demo and building it , itcame as:Build
1
1:20:55 PM 5/6/2014
Elapsed: 6 sec
Real-Time Workshop build procedure for method: 'entry Starting build procedure for model: BlinkBlueLed Starting Real-Time Workshop build procedure for model: BlinkBlueLed Model connectivity is: normal Create verification block: None Check Current Directory for building application. [&8;警告: Please change to STM32F4xx\STM32F4xxdemos\CodeGeneration build directory. In any other case there might be confilicts during the build-process towards finding desired files for creating the application.]&8;
Code Generation
Elapsed: 5 sec
Generating code into build folder: D:\Program Files\STMicroelectronics\STM32F4xx-MAT\STM32F4xx\STM32F4xxdemos\Test\BlinkBlueLed_stm32F4xx Real-Time Workshop build procedure for method: 'before_tlc before_tlc Top model: 'BlinkBlueLed Model: 'BlinkBlueLed Invoking Target Language Compiler on BlinkBlueLed.rtw Using System Target File: D:\Program Files\STMicroelectronics\STM32F4xx-MAT\STM32F4xx\rtw\stm32F4xx.tlc Loading TLC function libraries Initial pass through model to cache user defined code Caching model source code Warning: simMode value is 0.0 Warning: Create real-time application main.c Writing header file BlinkBlueLed.h Writing source file BlinkBlueLed.c Writing header file BlinkBlueLed_TimerPortAndPin.h Writing header file BlinkBlueLed_types.h Writing header file rtwtypes.h Writing header file BlinkBlueLed_private.h Writing source file main.c TLC code generation complete. Real-Time Workshop build procedure for method: 'after_tlc after_tlc Creating HTML report file Real-Time Workshop build procedure for method: 'before_make Code Format : Embedded-C Adding source and include directories to make process. STM32F4xx package install path: D:\PROGRA~1\STMICR~1\STM32F~1\STM32F~1 - additional source directories: D:\PROGRA~1\STMICR~1\STM32F~1\STM32F~1\lib\CMSIS\Device\ST\STM32F4xx\Source\Templates D:\PROGRA~1\STMICR~1\STM32F~1\STM32F~1\lib\STM32F4xx_StdPeriph_Driver\src D:\PROGRA~1\STMICR~1\STM32F~1\STM32F~1\src D:\PROGRA~1\STMICR~1\STM32F~1\STM32F~1\lib\CMSIS\Device\ST\STM32F4xx\Source\Templates\arm - additional include directories: D:\PROGRA~1\STMICR~1\STM32F~1\STM32F~1\lib\CMSIS\Device\ST\STM32F4xx\Include D:\PROGRA~1\STMICR~1\STM32F~1\STM32F~1\lib\CMSIS\Include D:\PROGRA~1\STMICR~1\STM32F~1\STM32F~1\lib\STM32F4xx_StdPeriph_Driver\inc D:\PROGRA~1\STMICR~1\STM32F~1\STM32F~1\src Processing Template Makefile: D:\Program Files\STMicroelectronics\STM32F4xx-MAT\STM32F4xx\rtw\stm32F4xx.tmf Wrapping unrecognized make command (angle brackets added) <''%MATLAB%\bin\%MATLAB_WIN_VER%\gmake''> in default batch file Creating BlinkBlueLed.mk from D:\Program Files\STMicroelectronics\STM32F4xx-MAT\STM32F4xx\rtw\stm32F4xx.tmf Building BlinkBlueLed: .\BlinkBlueLed.bat D:\Program Files\STMicroelectronics\STM32F4xx-MAT\STM32F4xx\STM32F4xxdemos\Test\BlinkBlueLed_stm32F4xx>set MATLAB=D:\Program Files\MATLAB\R2014a D:\Program Files\STMicroelectronics\STM32F4xx-MAT\STM32F4xx\STM32F4xxdemos\Test\BlinkBlueLed_stm32F4xx>''D:\Program Files\MATLAB\R2014a\bin\win32\gmake'' -f BlinkBlueLed.mk GENERATE_ASAP2=0 STM32TARGET=''STM32F4xxx'' TOOLPATHFROMREGISTRY=1 DONGLE=''STLinkV2'' COMPILERSETTINGS=''-c --cpu Cortex-M4.fp -g -O3 --apcs=interwork --split_sections $(INCLUDES)'' LINKERSETTINGS=''--cpu Cortex-M4.fp --map --list=$(MODEL)_KEIL_$(BOOT_MODE).map --scatter $(LDDIR)\$(STM32TARGET).sct --scanlib '' ASSEMBLERSETTINGS=''--via $(LDDIR)\asm.cmd'' DOWNLOADAPPLICATION=1 SIMULATION_MODE_RP=''NO_PIL'' TARGET_SRCS=''system_stm32f4xx.c stm32f4xx_gpio.c stm32f4xx_rcc.c stm32f4xx_flash.c stm32f4xx_pwr.c '' SYSTEM_SRCS=''stm32f4xx_it.c '' STARTUP_SRCS=''startup_stm32f4xx.s'' Makefile for KEIL BuildMode : real_time MODELREF_TARGET_TYPE=NONE SIMULATION_MODE_RP=NO_PIL MAKEFILEBUILDER_TGT=0 STANDALONE_SUPPRESS_EXE=0 Startup file: startup_stm32f4xx.o Startup path: ''D:\PROGRA~1\STMICR~1\STM32F~1\STM32F~1''\lib\CMSIS\Device\ST\STM32F4xx\Source\Templates\arm
Start compile .c source main.c
''main.c'', line 76: Error: 20: identifier ''TRUE'' is undefined OverrunFlags[0] = TRUE; ^ ''main.c'', line 84: Error: 20: identifier ''FALSE'' is undefined OverrunFlags[0] = FALSE; ^ main.c: 0 warnings, 2 errors gmake: *** [main.o] Error 1
I think the problem is caused by
/* Logical type definitions */
if
(!defined
(__cplusplus))ifndef
falsedefine
false (0U)endif
ifndef
truedefine
true (1U)endif
endif
in file
rtwtypes.h , but I can't figure it out.
So is thereany configuration I have missing ?
At the same time ,I've tried a thrid-party demo provided by Waijung14_03a and it works well.
Please help me . Thanks. stm32-mat/target-matlab-stm32f4