Skip to main content
9artus
Associate
May 10, 2014
Question

PORT and TIM issue with Discovery Board STM32F407

  • May 10, 2014
  • 4 replies
  • 846 views
Posted on May 10, 2014 at 16:47

I am working on a sine wave program as a part of an Amateur Radio project.  I have a working code producing what I want using TIM3-- PWM and PORTC.  I am unfortunately unable to neither change the TIM3 to any other TIM nor am I able to change my PORTC to PORTE.  The code follows closely the PWM example by STM and Andrew Markham's approach to the interrupt handle.  I can post code, although I am not sure of the proper messaging protocol for code in this forum.  Since the code is working fine using TIM3 and PORTC, I would have thought that either change would have been a simple task.  I have of course tried to change only one at a time.  Changes compile fine with no errors;  but no output is found on the appropriate pin using an oscilloscope, except the TIM3/PORTC arrangement. Thanks for any help.

Jack (W0FNQ)

 

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    May 10, 2014
    Posted on May 10, 2014 at 17:24

    You can paste source using the Format Code Block (Paintbrush [<>] icon). I want to see complete compilable code.

    Timers have specific pin utilization, so you can't randomly associate them. The part data sheet should show what routing options are available.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    9artus
    9artusAuthor
    Associate
    May 10, 2014
    Posted on May 10, 2014 at 19:15

    Thanks for reply. I am hoping to use TIM4 and PORTE pin 2. Here is the code:

    * Jack Generaux (W0FNQ)
    *
    * Some concepts and sine table from:
    ******************************************************************************
    * @file USART/main.c 
    * @author Andrew Markham
    * @version V1.0.0
    * @date 27-April-2012
    * @brief Main program body
    ******************************************************************************
    */ 
    /* Includes ------------------------------------------------------------------*/
    #include ''stm32f4xx_conf.h''
    #include <
    stdio.h
    >
    #include ''Oscillator.h''
    #include ''stm32f4xx.h''
    void PWM_Config(int period)
    {
    /* TIM3 clock enable */
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
    /* GPIOC and GPIOB clock enable */
    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC , ENABLE);
    /* GPIOC Configuration: TIM3 CH1 (PC6) */
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 ;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;
    GPIO_Init(GPIOC, &GPIO_InitStructure);
    /* Connect TIM3 pins to AF2 */
    GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_TIM3);
    /* No prescale, run at maximum frequency */
    uint16_t PrescalerValue=0;
    /* Time base configuration */
    TIM_TimeBaseStructure.TIM_Period = period;
    TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue;
    TIM_TimeBaseStructure.TIM_ClockDivision = 0;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
    /* PWM1 Mode configuration: Channel1 */
    TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
    TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
    TIM_OCInitStructure.TIM_Pulse = 0;
    TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
    TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Disable;
    TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Reset;
    TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCNIdleState_Reset;
    TIM_OC1Init(TIM3, &TIM_OCInitStructure);
    TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Enable);
    TIM_ARRPreloadConfig(TIM3, ENABLE);
    /* TIM3 enable counter */
    TIM_Cmd(TIM3, ENABLE);
    }
    void PWM_SetDC(uint16_t dutycycle)
    {
    TIM3->CCR1 = dutycycle;
    }
    void INTTIM_Config(void)
    {
    NVIC_InitTypeDef NVIC_InitStructure;
    /* Enable the TIM2 gloabal Interrupt */
    NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;
    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
    NVIC_Init(&NVIC_InitStructure);
    /* TIM2 clock enable */
    RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
    /* Time base configuration */
    TIM_TimeBaseStructure.TIM_Period = 10 - 1; // 1 MHz down to 100 KHz
    TIM_TimeBaseStructure.TIM_Prescaler = 84 - 1;
    TIM_TimeBaseStructure.TIM_ClockDivision = 0;
    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
    TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
    /* TIM IT enable */
    TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE);
    /* TIM2 enable counter */
    TIM_Cmd(TIM2, ENABLE);
    }
    void TIM2_IRQHandler(void)
    {
    if (TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET)
    {
    PWM_SetDC(pulse_width);
    // Calculate a new pulse width
    phase_accumulator+=R;
    angle=(uint8_t)(phase_accumulator>>24);
    pulse_width = sinetable[angle];
    TIM_ClearITPendingBit(TIM2, TIM_IT_Update);
    }

    Tesla DeLorean
    Guru
    May 10, 2014
    Posted on May 10, 2014 at 20:53

    PE2 has no timer associativity. Please refer to the

    http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00037051.pdf

    for your part.

    PE5/PE6 are TIM9_CH1 and CH2 respectively

    0690X00000605HcQAI.png

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    9artus
    9artusAuthor
    Associate
    May 10, 2014
    Posted on May 10, 2014 at 21:13

    thanks for the reference pointer.  I will explore other possible combinations.