Skip to main content
994724682
Associate
May 8, 2014
Question

STM32 VDE self-test library for stdperiph_lib

  • May 8, 2014
  • 8 replies
  • 1497 views
Posted on May 08, 2014 at 09:28

Dear ST;

I want to Optimize my program,so for the safety,I need the self-test library.but I can not find it on the st.com,so I come here to get help from you guys. Thanks very much.

Yours,

liuwei

#stm32f10x #stm32 #certification #vde
This topic has been closed for replies.

8 replies

frankmeyer9
Associate III
May 8, 2014
Posted on May 08, 2014 at 10:02

I want to Optimize my program,so for the safety,I need the self-test library

 

I'm not aware that any such thing exists for STM32.

If you need safety features, I suggest to have a look at Cortex R controllers (like the TI Hercules series) which, AFAIK, implement such features in hardware.

994724682
994724682Author
Associate
May 8, 2014
Posted on May 08, 2014 at 10:09

I'm quite that the library exists. I found some people also look for it.but there is  no answer.I hope I can get what I want. 

994724682
994724682Author
Associate
May 8, 2014
Posted on May 08, 2014 at 10:10

quite sure

frankmeyer9
Associate III
May 8, 2014
Posted on May 08, 2014 at 10:18

I'm quite that the library exists. I found some people also look for it.but there is  no answer.I hope I can get what I want. 

 

Seems you are right, only that ST provides it just to ''selected'' customers.

But having seem SIL3 device solutions with two identical MCUs, specialized MCU which support that features in hardware seem a better solution to me.

994724682
994724682Author
Associate
May 8, 2014
Posted on May 08, 2014 at 10:46

I have got one from some people long time ago,but it is too old,it's 1.2 version , now the firmware library is 3.5 version ,it has a big difference to the old version, I'm not really understand about the cpu inside things,so I can not transplant it .the question bothered me for a long time...

Tesla DeLorean
Guru
May 8, 2014
Posted on May 08, 2014 at 13:12

Put in a request with your local ST rep or FAE, the forum is not the place to secure limited distribution or NDA'd material.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
994724682
994724682Author
Associate
May 13, 2014
Posted on May 13, 2014 at 09:25

I sent to the requesting agency ST companies are basically ignored, did not respond. So I wanted to see if I can get the answer here.

Montassar BEN ROMDHANE_O
Visitor II
May 14, 2014
Posted on May 14, 2014 at 17:33

Hi,

Sorry, the STM32F10x_StdPeriph_Lib_V3.5.0 is not certified by VDE.

For more information please refer to this application note:

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/CD00290100.pdf

With regards.