Skip to main content
fshah48
Associate II
April 6, 2017
Question

Want to generate pulse train of progressively increasing pulse duration in response to trigger train.

  • April 6, 2017
  • 5 replies
  • 1060 views
Posted on April 06, 2017 at 11:50

Want to generate pulse train of progressively increasing pulse duration in response to a trigger train. OPM seems o be solution. Can I change CCR1 and ARR register values in interrupt routine to change 'delay' and 'pulse duration'?

    This topic has been closed for replies.

    5 replies

    Tesla DeLorean
    Guru
    April 6, 2017
    Posted on April 06, 2017 at 15:06

    >>Can I change CCR1 and ARR register values in interrupt routine to change 'delay' and 'pulse duration'?

    Yes, typically in the Update handler, with the shadowing you are one period behind. Set the pulse width to zero to turn off.

    The advanced timers also have a repetition count, so multiple pulses can be sent between Update interrupts.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    fshah48
    fshah48Author
    Associate II
    April 6, 2017
    Posted on April 06, 2017 at 20:56

    Hi Clive

    Le me make the problem a bit more clear. I have a trigger waveform approx

    20ms period with 50% duty cycle. I must generate a constant width pulse on

    each trigger edge but progressively decreasing delay.

    I don't understand 'shadowing'?

    I was hoping to set CCR1 and ARR to starting values, and decrease CCR1 and

    ARR registers in the handler. Hoping to get output pulses of constant

    width(100us) and varying delay (starting from 8000us down to 20us.

    fshah48

    On Thu, Apr 6, 2017 at 6:07 PM, Clive One <st-microelectronics@jiveon.com>

    Tesla DeLorean
    Guru
    April 6, 2017
    Posted on April 06, 2017 at 22:04

    Shadowing just means it starts using the new data at zero phase angle (update), rather than some random time within the current cycle, which could glitch the pulse width.

    If the pulse width remains constant, then you don't need to reprogram CCR1. Have DMA load ARR automatically at Update, and have a memory table describing smaller and smaller values for the Period. Or use the IRQ.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    S.Ma
    Principal
    April 6, 2017
    Posted on April 06, 2017 at 21:41

    How about a one shot timer mode triggered by channel input 1 or 2, and output pulse value is set by a serial table pushed by dma on the output compare register to ouput gpios? Would work even with khz periodic signals...