Skip to main content
ArturasV
Associate III
January 26, 2017
Solved

STM32L011K4+LSM9ds1tr SPI wrong readings

  • January 26, 2017
  • 15 replies
  • 2507 views
Posted on January 26, 2017 at 13:31

Hello, we are having problems with communicating to sensor LSM9ds1tr via SPI with sm32l011k4 mcu. The problem is that SPI seems to work good and looking with logic analyzer proves that everything is okey, we are seeing exactly the same thing as mcu reads. We are trying to read the WHO_AM_I register of accelerometer/gyroscope and magnetometer and for some reason we read wrong values compared to the datasheet. According to the data sheet, then reading ACC/Gyro  WHO_AM_I register the value should be 0x68 and then reading Magnetometer WHO_AM_I register the value should be 0x3D. However, when reading these, we always get 0x40 when reading accelerometer/gyro register and we always get 0x38 when reading magnetometer WHO_AM_I register. Could anyone help us to solve the problem and point out what we are doing wrong? I attach the schematics of the sensor, spi initialization code and our reading function + snapshots from logic analyzer. 0690X00000605wbQAA.png0690X0000060698QAA.png0690X000006069DQAQ.png

/*

* @brief: function to configure SPI1 peripheral.

* (1) Set MCU as a master, configure baud rate to fpclk/256

* (2) Slave select output enable

* (3) Enable SPI1 peripheral.

*/

void spi_config(void)

{

SPI1->CR1 = SPI_CR1_MSTR | SPI_CR1_BR; /* (1) */

SPI1->CR2 = SPI_CR2_SSOE; /* (2) */

SPI1->CR1 |= SPI_CR1_SPE; /* (3) */

}

/*

* @brief: function to read data from slave via SPI.

* @params: arg1 - reg_ptr: address of the register which you want to read

* arg2 - b_count: number of bytes to read starting from the address given by reg_ptr.

* (1) Create local variable called index, to follow read byte number

* (2) Chip select goes to low level

* (3) Write value to the SPI Tx buffer

* (4) Wait until data is transmitted and Tx fifo is empty

* (5) Wait until Rx fifo is not empty (means some data is received).

* (6) Read received Data.

* (7) Start a loop with number of iterations equal to arg2.

* (8) Send dummy byte so master generates clock for the communication

* (9) Small delay before setting CS back to high

* (10) Chip select goes to high level

* ----------------------------------------------------------------------------------------------

* @Note: Delay (9) will change when changing mcu clock settings

*/

void spi_read_acc(uint8_t reg_ptr, uint8_t b_count)

{

uint8_t index = 0; /* (1) */

GPIOB->ODR &= ~0x20; /* (2) */

SPI1->DR = reg_ptr; /* (3) */

while(!(SPI1->SR & 0x02)); /* (4) */

while(!(SPI1->SR & 0x01)); /* (5) */

spi_rx_data[index++] = SPI1->DR; /* (6) */

for(; index < b_count + 1; index++) /* (7) */

{

SPI1->DR = 0xFF; /* (8) */

while(!(SPI1->SR & 0x02)); /* (4) */

while(!(SPI1->SR & 0x01)); /* (5) */

spi_rx_data[index] = SPI1->DR; /* (6) */

}

for(index = 0; index < 20; index++); /* (9) */

GPIOB->ODR |= 0x20; /* (10) */

}

&sharpdefine LSM9DS_WHO_AM_I 0x0F

int main(void)

{

hardware init(); // pseudo code

// ...

spi_read_acc(LSM9DS_WHO_AM_I | 0x80, 1);

while(1);

}

#stm32l011k4 #lsm9ds1
This topic has been closed for replies.
Best answer by T J
Posted on January 31, 2017 at 23:16

Wow, when you zoom into the logic analyzer image there is much more detail...

over 55 now, eyesight with focusing is difficult.

I can see on the data sheet, that address 0x1F looks suspiciously like your data...

try reading registers 0x21,0x22,0x23...

your CPOL and CPHA look good.

how long is the data cable ?

what speed are you running, 10khz ? this should be no problem.

where did you buy the chips ?

do you think they could be counterfeit ?

I have been touched by counterfeit product a few times...

Pins 7 and 8 should be low, did you check that ?

what is pin 13 all about ?  no details in this sheet, looks like it needs to go high.

15 replies

ArturasV
ArturasVAuthor
Associate III
January 29, 2017
Posted on January 29, 2017 at 11:39

Any suggestions anyone? We still are struggling with this problem.

waclawek.jan
Super User
January 29, 2017
Posted on January 29, 2017 at 13:32

You might consider posting this question in the

https://community.st.com/community/mems-sensors-community/mems-sensors-forum/content

forum.

JW

ArturasV
ArturasVAuthor
Associate III
January 29, 2017
Posted on January 29, 2017 at 15:01

Thank you for your comment JW. Can forum admin move this to the 'Sensors and MEMS forum'? Or i can just repost this there?

waclawek.jan
Super User
January 29, 2017
Posted on January 29, 2017 at 21:59

You should be able to move it yourself: on the right upper side just below your avatar there should be an 'Actions' pulldown, and in that a 'Move'.

JW

T J
Senior III
January 29, 2017
Posted on January 29, 2017 at 15:05

this works for the '091

void quickSendReceive8SPI(SPI_HandleTypeDef *hspi){ while( !( hspi->Instance->SR & SPI_FLAG_TXE)); *((__IO uint8_t *)&hspi->Instance->DR) = TxSPIByte; // force the SPI to transceive 8 bit while( !( hspi->Instance->SR & SPI_FLAG_TXE)); while( ( hspi->Instance->SR & SPI_FLAG_BSY)); while( ( hspi->Instance->SR & SPI_FLAG_RXNE)) RxSPIByte1 = hspi->Instance->DR; }�?�?�?�?�?�?�?�?�?�?

T J
Senior III
January 29, 2017
Posted on January 29, 2017 at 22:09

I can see it exactly in your code,

#define SPI_SR_RXNE                /*!< 0x00000001 */

#define SPI_SR_TXE                 /*!< 0x00000002 */

#define SPI_SR_BSY                  /*!< 0x00000080 */

You are not checking that the TX is still busy..

Sure the Txbuffer is empty, but the transmission  is still in progress.

between lines (4) and (5) above...

add:

while(!(SPI1->SR & 0x02)); /* (4) */

while( SPI1->SR & 0x80 ); /* (4a) */

while(!(SPI1->SR & 0x01)); /* (5) */
ArturasV
ArturasVAuthor
Associate III
January 30, 2017
Posted on January 30, 2017 at 14:12

Hello Marsh.Nick, thank you for your answer. We tried to apply your suggestion, however sensor still responds with the same values as previously. So obviously waiting until Tx is not bussy is not the problem here. Any more ideas? Could it possible be something wrong with our SPI configuration? 

T J
Senior III
January 30, 2017
Posted on January 31, 2017 at 00:57

Hi,

If you can check my code above that works on the '091 bxCan peripheral, you will see it is almost exactly the same as yours

did you notice that you needed to insert that line (4a)  twice ?

other than that, I used the CubeMX to initialise the SPI port.

ArturasV
ArturasVAuthor
Associate III
January 31, 2017
Posted on January 31, 2017 at 17:04

Yes, we are aware that we had to change the code in two spots. We actually tried today the piece of code which you showed above and it gave the same results. We are considering to change the chip to another. Maybe you have any more ideas? Thank you for your answers.

T J
Senior III
January 31, 2017
Posted on January 31, 2017 at 21:55

Hi,

Can you see the data on the Logic analayser ?

did you check the CPOL and CPHA bits ?

my code works for the bxCAN embedded peripheral used in the '091.

waclawek.jan
Super User
January 31, 2017
Posted on January 31, 2017 at 22:54

Nick,

Can you see the data on the Logic analayser ?

Look at the original post.

Arth,

Until somebody more knowledgeable from ST chimes in:

I went through publicly available code and all I could find were the same values as in the DS. I also browsed through all the ST MEMS datasheets and compiled the WHO_AM_I responses for various parts (www.efton.sk/STM32/st_mems_whoami.txt) but there is nothing resembling your combination of responses.

What exactly is your hardware? Is it a genuine ST part?

JW

T J
T JBest answer
Senior III
January 31, 2017
Posted on January 31, 2017 at 23:16

Wow, when you zoom into the logic analyzer image there is much more detail...

over 55 now, eyesight with focusing is difficult.

I can see on the data sheet, that address 0x1F looks suspiciously like your data...

try reading registers 0x21,0x22,0x23...

your CPOL and CPHA look good.

how long is the data cable ?

what speed are you running, 10khz ? this should be no problem.

where did you buy the chips ?

do you think they could be counterfeit ?

I have been touched by counterfeit product a few times...

Pins 7 and 8 should be low, did you check that ?

what is pin 13 all about ?  no details in this sheet, looks like it needs to go high.

ArturasV
ArturasVAuthor
Associate III
February 1, 2017
Posted on February 01, 2017 at 15:19

Hey marsh.Nick, thanks for your answer. We bought the chips from Mouser so we don't think they could be counterfeit. And yes we checked everything you have said. We are now thinking that maybe we could have damaged the chips when soldering them on the pcb, because today we tried the same software with another accelerometer and that one works perfectly. Anyway new chips are on their way, i'll give you a feedback as soon as we test the new ones. They should reach us this friday/monday.

ArturasV
ArturasVAuthor
Associate III
February 8, 2017
Posted on February 08, 2017 at 19:17

Just wanted to thank you guys for your ideas and time. We believe that we may have damaged the chip while soldering these sensors on pcb. Received a new ones yesterday, soldered them on the same pcb and everything is working as expected, we are getting correct values now. We do not think that the part was fake since we bought it from Mouser, so probably it is our fault. Thank you everyone again, regards.