Skip to main content
mark239955_st
Visitor II
May 23, 2014
Solved

SPC564B70 (Bolero) Power Draw in Standby Mode

  • May 23, 2014
  • 1 reply
  • 1104 views
Posted on May 23, 2014 at 19:21

Can anybody offer any knowledge of using STANDBY mode? 

I am putting the chip in STANDBY and it appears to go there, as the processor goes dormant until I cause a wakeup event.  But the current draw on the VDD_LV power-input (2.1v) is ridiculously high (~100ma).   I've confirmed that the power is not going out the ports - those are all ok - it appears to be going to core/peripherals (hence VDD_LV). 

Following the spec carefully, with weeks of scrutiny and experimentation.   Can give more details if anybody has experience here...

tnx,

-mark

#powerconsumption-power-standby
This topic has been closed for replies.
Best answer by Erwan YVIN
Posted on May 27, 2014 at 10:58

Hello Mark ,

sorry for our late answer.

you can check in the chapter : (cf reference manual of SPC564B70 (Bolero))

Table 88. Low-Power Peripheral Configuration Registers (ME_LP_PC0…7) Field Descriptions

Peripheral control during STANDBY

0 Peripheral is frozen with clock gated

1 Peripheral is active

And your peripheral control registers are maybe badly configured.

   Best regards

                Erwan YVIN

1 reply

Erwan YVIN
Erwan YVINBest answer
ST Technical Moderator
May 27, 2014
Posted on May 27, 2014 at 10:58

Hello Mark ,

sorry for our late answer.

you can check in the chapter : (cf reference manual of SPC564B70 (Bolero))

Table 88. Low-Power Peripheral Configuration Registers (ME_LP_PC0…7) Field Descriptions

Peripheral control during STANDBY

0 Peripheral is frozen with clock gated

1 Peripheral is active

And your peripheral control registers are maybe badly configured.

   Best regards

                Erwan YVIN

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.