Question
FLASH_WaitForLastOperation CubeMx error
Posted on January 23, 2017 at 10:02
The latest Version of CubeMx (4.19.0) the 'FLASH_WaitForLastOperation' function causes errors if the HAL_GetTick() function is near its rollover point. The cause seems to be 'uint32_t timeout = HAL_GetTick() + Timeout', which causes an error of the comparison 'HAL_GetTick() >= timeout'. With a 1ms resolution the error happens after 49 days, which could cause a serious problem in real systems. It would be nice, if this could be corrected.
best regards
Thomas
#cubemx