Skip to main content
mats23
Associate III
Oct 9, 2014 2:59 PM UTC
Question

Touchscreen and I2C bus on STM32F429I DISCO

Posted on October 09, 2014 at 16:59

Hi,

I am running on an STM32F429I DISCO board and are trying to get the touchscreen to work in an application using the I2C bus, but I cannot get the touchscreen to run at the same time as the I2C.

For the I2C bus I use the PA8, PC9 pins, i.e. the I2C3, as this seemed to be the only I2C bus on this board with free pins.

Is there anything fundamental on this board preventing me from doing what I want to do, or am I just doing something wrong?

Many thanks for any hints.

Regards, Mats
    This topic has been closed for replies.

    1 reply

    mats23
    mats23Author
    Associate III
    Oct 31, 2014 12:11 PM UTC
    Posted on October 31, 2014 at 13:11

    Finally I think I got this up and running. I had to modify my i2c init function and it now looks like this:

    I2cHandle->Instance = I2Cx;
    I2cHandle->Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; 
    I2cHandle->Init.ClockSpeed = 100000; 
    I2cHandle->Init.DualAddressMode = I2C_DUALADDRESS_DISABLED; 
    I2cHandle->Init.DutyCycle = I2C_DUTYCYCLE_2; 
    I2cHandle->Init.GeneralCallMode = I2C_GENERALCALL_DISABLED;
    I2cHandle->Init.NoStretchMode = I2C_NOSTRETCH_DISABLED; 
    I2cHandle->Init.OwnAddress1 = 0; 
    I2cHandle->Init.OwnAddress2 = 0;