Skip to main content
chernobay
Associate II
April 11, 2016
Question

Debugging STM32F042 in Keil

  • April 11, 2016
  • 4 replies
  • 1039 views
Posted on April 11, 2016 at 23:05

I have a problem with loading into debugger in Keil for STM32F042

(Run to main() is off)

- normal start for example from STM32F0xx_StdPeriph_Lib_V1.5.0\Projects\STM32F0xx_StdPeriph_Examples

for STM32F030

http://i.piccy.info/i9/09aee8af9c0c9198abe58d073d09447a/1460406714/61602/1024043/030.png

anf this for STM32F042

http://i.piccy.info/i9/c1d5347c947628a4685b462e2021c855/1460406728/63733/1024043/042.png

How do I start from  0x080000C8 for the STM32F042?

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    April 12, 2016
    Posted on April 12, 2016 at 03:48

    Make sure that the BOOT pin is low if you want it to start in FLASH

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    chernobay
    chernobayAuthor
    Associate II
    April 12, 2016
    Posted on April 12, 2016 at 10:37

    Thank you, clive1.

    If PA8(BOOT0) is pull down - all is OK.

    chernobay
    chernobayAuthor
    Associate II
    April 14, 2016
    Posted on April 14, 2016 at 12:23

    With configure of system memory with ST-LINK Utility all is OK 

    http://arm-stm.blogspot.com/2016/04/stm32f0-stm32f042-boot-problem-user.html

    chernobay
    chernobayAuthor
    Associate II
    December 10, 2016
    Posted on December 10, 2016 at 07:27

    You can set  User Option bit - nBoot0 

    https://arm-stm.blogspot.com/2016/04/stm32f0-stm32f042-boot-problem-user.html