Question
designing ISP header for STM32F030F4P6
Posted on June 06, 2014 at 07:36
Hello,
I am designing a board using STM32F030F4P6. I have to use STM32F0 Discovery board STLINK for ISP. Checking the schematics of Discovery board, I found out that the ISP connector (SWD) is connected as follows: 1.3.3V 2.SWCLK 3.GND 4.SWIO 5.NRST 6.PB3 of the STM32 controller on board. Now, I have trouble understanding the 6th connection. the signal name is given as T_SWO and it is connected to PB3. what is this signal? In TSSOP 20 package of STM32F030F4P6, this pin(PB3) is not there. so where should I connect 6th pin of ISP header? or can i leave it open? Referances: MB1034: Discovery board schema DM00088500.pdf: STM32F030F4P6 Datasheet DM00039193.pdf:STM32F051xx Datasheet #stm32f03x6