stm32l496g_discovery_sd.c hypothesis denied
Bugs in current, and older code trees
STM32Cube_FW_L4_V1.12.0\Drivers\BSP\STM32L496G-Discovery\stm32l496g_discovery_sd.c
...
/**
* @brief Initializes the SD MSP. * @note The SDMMC clock configuration done within this function assumes that * the PLLSAI1 input clock runs at 8 MHz. * @param hsd: SD handle * @param Params: Additional parameters * @retval None */__weak void BSP_SD_MspInit(SD_HandleTypeDef *hsd, void *Params){ GPIO_InitTypeDef gpioinitstruct = {0}; RCC_PeriphCLKInitTypeDef RCC_PeriphClkInit;/* Prevent unused argument(s) compilation warning */
UNUSED(Params);HAL_RCCEx_GetPeriphCLKConfig(&RCC_PeriphClkInit);
/* Configure the SDMMC1 clock source. The clock is derived from the PLLSAI1 */
/* Hypothesis is that PLLSAI1 VCO input is 8Mhz */ RCC_PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_SDMMC1; RCC_PeriphClkInit.PLLSAI1.PLLSAI1N = 24; RCC_PeriphClkInit.PLLSAI1.PLLSAI1Q = 4; RCC_PeriphClkInit.PLLSAI1.PLLSAI1ClockOut = RCC_PLLSAI1_48M2CLK; RCC_PeriphClkInit.Sdmmc1ClockSelection = RCC_SDMMC1CLKSOURCE_PLLSAI1; if (HAL_RCCEx_PeriphCLKConfig(&RCC_PeriphClkInit) != HAL_OK) { while (1) {} }...
The PLL share a common divided clock source via PLLM, in the critical example code for this platform the source is almost always the MSI in Range 6, ie 4 MHz and not an 8 MHz HSE
Resulting in the microSD card being super slow in the primary demo code, 24 MHz at the peripheral, 12 MHz on the wire, instead of twice that.
STM32Cube_FW_L4_V1.12.0\Projects\32L496GDISCOVERY\Applications\FatFs\FatFs_uSD_Standalone\Src\main.c
...
/**
* @brief System Clock Configuration * The system Clock is configured as follows : * System Clock source = PLL (MSI) * SYSCLK(Hz) = 80000000 * HCLK(Hz) = 80000000 * AHB Prescaler = 1 * APB1 Prescaler = 1 * APB2 Prescaler = 1 * MSI Frequency(Hz) = 4000000 * PLL_M = 1 * PLL_N = 40 * PLL_R = 2 * PLL_P = 7 * PLL_Q = 4 * Flash Latency(WS) = 4 * @param None * @retval None */void SystemClock_Config(void){ RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; RCC_OscInitTypeDef RCC_OscInitStruct = {0};/* MSI is enabled after System reset, activate PLL with MSI as source */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI; RCC_OscInitStruct.MSIState = RCC_MSI_ON; RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6; RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI; RCC_OscInitStruct.PLL.PLLM = 1; RCC_OscInitStruct.PLL.PLLN = 40; RCC_OscInitStruct.PLL.PLLR = 2; RCC_OscInitStruct.PLL.PLLP = 7; RCC_OscInitStruct.PLL.PLLQ = 4; if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { /* Initialization Error */ while(1); }...