Skip to main content
Cooke.Ernest
Associate III
October 4, 2017
Question

SPWF01SA - Setting the IP Address

  • October 4, 2017
  • 0 replies
  • 563 views
Posted on October 04, 2017 at 14:34

Hi,

I have recently just started working on Wi-Fi code on the SPWF01SA module using the STM32F1 Nucleo Development Board.

I was able to get the various configuration values from the Wi-Fi module using the functions below.

 0690X00000608TUQAY.png

And I displayed these values in HyperTerminal as can be seen below:

0690X00000608N9QAI.png

Is it possible to change the IP address of the module from the default value (192.168.0.58) to another IP address?

If it is possible, can someone explain to me how it is done?

Thank You,

Ernest

#wifi-module #wifi-usart #stm32f1-nucleo #idw001v1 #spwf01sa1 #wifi-spwf01sa
This topic has been closed for replies.