2015-08-07 8:21 PM
Hi! Device is STM32F103C8
A update event from TIM4 is used to trigger DMA channel7 who then is supposed to transfer 9 values in circular mode to TIM3 CCR1. However the DMA transfers only one value and that one is set to 0 and the rest is set to 127!? So what i get is narrow pulse on CCR1 going round at the speed of TIM4 update event.1.
#include ''stm32f10x.h'' 2. uint8_t buffer[9] = {0,16,32,48,64,80,96,112,127};void tim4(void) { /************************* Tim4 ****************************************************/ TIM4->CCMR1 |= 0b0110000001100000; //OCM1 is set to PWM1 mode and OCM2 is set to PWM1 mode TIM4->CCMR2 |= 0b0110000001100000; //OCM3 is set to PWM1 mode and OCM4 is set to PWM1 mode TIM4->CCER |= TIM_CCER_CC1E; //Capture/Compare 1 output enable TIM4->CCER |= TIM_CCER_CC2E; //Capture/Compare 2 output enable TIM4->CCER |= TIM_CCER_CC3E; //Capture/Compare 1 output enable TIM4->CCER |= TIM_CCER_CC4E; //Capture/Compare 2 output enable TIM4->PSC = 8192; TIM4->ARR = 1; TIM4->CCR1 = 1; //CCR1 register set to initial PWM1 value TIM4->CCR2 = 1; //CCR2 register set to initial PWM2 value TIM4->CCR3 = 1; TIM4->CCR4 = 1; TIM4->DIER |= TIM_DIER_UDE; //DMA request on tim4 Update event TIM4->BDTR |= TIM_BDTR_MOE; //Enable output stage //TIM4->CR2 |= TIM_CR2_CCDS; //DMA request on Update event TIM4->CR1 |= TIM_CR1_CEN; //Enable Timer4 }
void tim3( void ) { /************ Tim3 ********************************************************************/ TIM3->CCMR1 |= 0b0110000001100000; //OCM1 is set to PWM1 mode and OCM2 is set to PWM1 mode TIM3->CCMR2 |= 0b0110000001100000; //OCM3 is set to PWM1 mode and OCM4 is set to PMW1 mode TIM3->CCER |= TIM_CCER_CC1E; //Capture/Compare 1 output enable TIM3->CCER |= TIM_CCER_CC2E; //Capture/Compare 2 output enable TIM3->CCER |= TIM_CCER_CC3E; //Capture/Compare 3 output enable TIM3->CCER |= TIM_CCER_CC4E; //Capture/Compare 4 output enable TIM3->PSC = 0; TIM3->ARR = 127; TIM3->CCR1 = 64; //CCR1 register set to initial PWM1 value TIM3->CCR2 = 64; //CCR2 register set to initial PWM2 value TIM3->CCR3 = 64;<br> TIM3->CCR4 = 64;<br> TIM3->BDTR |= TIM_BDTR_MOE; //Enable output stage TIM3->CR1 |= TIM_CR1_CEN; //Enable Timer3 }
void dma1( void ) { /**************** DMA configuration......DMA ch7 triggered by TIM4 UD ***********************************/ DMA1_Channel7->CCR = 0; //Reset CCR DMA1->IFCR = 0; //Clear all pending (old) DMA1 Stream's interrupts DMA1_Channel7->CNDTR = 9; //Number of DMA transfers DMA1_Channel7->CMAR |= (uint32_t)&buffer; //Source, should fetch data from buffer!??! DMA1_Channel7->CPAR |= (uint32_t)&(TIM3->CCR1); //Destination, TIM3 CCR1 //DMA1_Channel7->CCR |= DMA_CCR7_PSIZE_0; //Set peripheral size to 16bits //DMA1_Channel7->CCR |= DMA_CCR7_MSIZE_0; //Set memory size to 16bits DMA1_Channel7->CCR |= DMA_CCR7_DIR; //Read from memory to peripheral DMA1_Channel7->CCR |= DMA_CCR7_MINC; //Memory increment enabled //DMA1_Channel7->CCR |= DMA_CCR7_MEM2MEM; //Memory to memory enabled //DMA1_Channel7->CCR |= DMA_CCR7_PINC; //Peripheral increment enabled DMA1_Channel7->CCR |= DMA_CCR7_CIRC; //DMA set to circular mode DMA1_Channel7->CCR |= DMA_CCR7_PL; //Channel Priority level set to very high DMA1_Channel7->CCR |= DMA_CCR7_EN; //DMA channel7 enabled }
2015-08-08 1:35 PM
Check the DMA channel - NDTR should change as TIM4 updates happen. Check also the DMA error flags.
Maybe the following kicked in: RM0008, 4: The peripheral registers can be accessed by half-words (16-bit) or words (32-bit). Minor remarks:DMA1_Channel7->CMAR |= (uint32_t)&buffer; 
//Source, should fetch data from buffer!??!
DMA1_Channel7->CPAR |= (uint32_t)&(TIM3->CCR1); 
//Destination,2015-08-08 5:11 PM
Yes your right Jan, removed TIM4_BDTR and TIM3_BDTR and |
When i change CCR7_PSIZE and CCR7_MSIZE from 8 to , 16 or 32 all i get is a change of number of high and low states on TIM3 CCR1 pin , no actual fetch of values from the array seams to happen. But the number of transactions correlates with the number of update events when i look on the oscilloscope. In 13.3.5 Error management it says: >When a DMA transfer error occurs during a DMA read or a write access, the faulty channel is automatically disabled through a hardware clear of its EN So since CCR1 emits signals in sync with TIM4 update events DMA ch7 is not disabled and is working, if not the channel would be disabled and TEIF7 be set and no signals on CCR1 would be seen.