Skip to main content
paul2
Associate III
July 8, 2014
Question

STM32F4 - trigger digital output based on ADC - minimizing delays

  • July 8, 2014
  • 3 replies
  • 922 views
Posted on July 08, 2014 at 09:30

Hi,

I’m trying to minimize control loop delays. Based on a certain analog value (adjustable threshold) a digital output is triggered. Reading ADC values is done by using DMA, digital outputs are driven without DMA.

Results measured by scoop: minimum delay ~300 μs, variation ~90 μs (min

300 μs,

max

390 μs

)

Does anybody have some tips/tricks/best practices minimizing ADC-DO control loop delays?

Thanks.

    This topic has been closed for replies.

    3 replies

    chen
    Associate II
    July 8, 2014
    Posted on July 08, 2014 at 10:26

    Hi

    ''

    I’m trying to minimize control loop delays. Based on a certain analog value (adjustable threshold) a digital output is triggered. Reading ADC values is done by using DMA, digital outputs are driven without DMA.

    ''

    ''

    Does anybody have some tips/tricks/best practices minimizing ADC-DO control loop delays?

    ''

    Not sure what you mean by 'ADC control loop' ??

    Try looking at the 'Analogue Watchdog' feature of the ADC.

    It is basically 2 threshold values which can trigger an IRQ

    frankmeyer9
    Associate III
    July 8, 2014
    Posted on July 08, 2014 at 11:21

    Why not using a discrete comparator, or a stm32f3 with integrated comparators ?

    That would remove much software-induced delays from the loop.

    For better suggestions, you might perhaps reveal more details about your application.

    Tesla DeLorean
    Guru
    July 8, 2014
    Posted on July 08, 2014 at 13:22

    A singular ADC value, how frequently? Perhaps you could avoid DMA, or use an alternate ADCx unit, and use the EOC interrupt to read/process the threshold

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..