Skip to main content
maggie
Associate III
October 10, 2014
Question

STM32F4 Cube-based USB Device Microphone in Audio Class streaming to Host PC

Posted on October 10, 2014 at 04:04

Hi,

Ideally, I'd like to have a firmware that has the following support:

  1. Cube-based
  2. Works in STM32F4
  3. Works as a dual-mode USB Device (not Host) in Audio Device Class, where these 2 endpoints are configured:

  • (a) 1 isochronous IN endpoint to handle audio coming from a host PC (to act as speaker)
  • (b) 1 isochronous OUT endpoint to handle audio coming out to a host PC (to act as microphone)

I already have a firmware that satisfies (1), (2) and (3.a) which is described in another

/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F4Discovery%20Cube-based%20USB%20Speaker%20application%20not%20working&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=116

, but I'm having problems accomplishing (3.b).

Of course I already checked the ''Audio_playback_and_record'' common among STM32F4 and available in STM32CubeF4 package, however, the recording part there is configured as USB Host, not to mention that the USB Class is Mass Storage Class, not Audio Device Class.

I can see related post

/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/USB%20Audio%20Device%20with%20I2S%20microphone&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&currentviews=2355

, but no conclusive answers (there was one saying he was able to do it but no details as to how were posted).

At this

/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F4Discovery%20Cube-based%20USB%20Speaker%20application%20not%20working&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=116

post, I was informed by someone from the Cube team that there isn't such a program yet for USB Device microphone where audio is configured to go to host PC (as of September 2014).

However,

/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/USB%20Audio%20Device%20with%20I2S%20microphone&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&currentviews=2355

post I mentioned reached almost 2400 views, so that only means many people are searching for the same topic and still searching answers up until now (no other posts have more info aside from this one)...

So I created this post.

Anyone who can provide reference for us to allow STM32F4 to support ''USB Device microphone where audio is configured to go to host PC''?

Any reference that could give us a jump start would do - then we can keep this thread rolling.

BTW, I have STM32F4-Discovery with STM32F407VGx on hand.

Since it has on-board CS43L22 DAC, a MP45DT02 MEMS microphone, DAC OUT for earphones, and of course USB Device mode port - it's the perfect device I can use for evaluation.

Thanks in advance to those who can contribute to this post.

Regards,

Maj

#stm32cubef4-usb-microphone-audio
This topic has been closed for replies.

11 replies

Montassar BEN ROMDHANE_O
Visitor II
October 13, 2014
Posted on October 13, 2014 at 11:10

Hi Maj,

We'll let our development team know about your suggestion.

Regards,

Heisenberg.

maggie
maggieAuthor
Associate III
October 14, 2014
Posted on October 14, 2014 at 09:10

To Heisenberg

- please let us know once the development team released this in the future versions of STM32CubeF4 examples, via posting to this thread.

I know it would be a hassle (sorry), but I'm saying for the benefit of all those who browses this forum, so that we/they can link the answer via your future post (ie ''this is already released as part of STM32CubeF4 vX.X...'').

To all other users

 - if you were able to make a firmware successfully with this setup, please still feel free to post.

Thank you very much!

delphi
Associate II
August 3, 2016
Posted on August 03, 2016 at 19:29

That sound good! We must give a lot of critics to ST engineers. They must introduce such example! I insist on that!

marek2399
Associate III
May 27, 2018
Posted on May 27, 2018 at 15:19

Well, so two years and nothing? Really ST engineers? Awsome job. Till now i was really glad to use STM but their support starts to be really terrible.

TWong.11
Visitor II
November 30, 2018

I've been struggling for weeks to implement audio upstreaming feature on a stm32f103 board with cube generated codes, I can only stream lagging and intermittent sounds by using USBD_LL_Transmit() at DATAIN stage for now, I'm going really desperate.. And why are such basic examples nowhere to be found.

waclawek.jan
Super User
November 30, 2018

Maybe because it's not that basic to get it right. You've just told it: you've made the basic example stitching up ready made pieces of code, and the result is less than satisfactory.

JW

MAdur
Visitor II
February 7, 2019

Good one, @maggie​ 

I am starting to try to do almost the same thing on a STM32F7. Have you had any progress?

Gabriel Melo
Associate II
July 24, 2019

Did anyone get it to work already? I got some luck using X-CUBE-MEMS1 package, the device is recognized as a mic; however, when I try to send samples I get some very strange results and noisy samples.

The way I did it I just used the usbd_audio_in.h and .c files instead of the default usbd_audio.h and .c provided by ST (and calling the initialization and send functions).

Klang.Martin
Associate II
January 17, 2020

I've been looking for a USB microphone example for a long time. I've done my own solution, but calling USBD_LL_Transmit from the DataIn callback doesn't seem very clean, and it means I can't send MIDI messages while streaming audio which is a big issue for some of my use cases.

Then today I found this: X-CUBE-USB-AUDIO

It has a complete example with audio record, playback, and feedback. It's pretty complex! Disappointingly it also calls USBD_LL_Transmit from DataIn, and of course there's no MIDI support.

To be honest I have no idea how you are supposed to use the Cube expansion packages. It doesn't show up when I do Manage Embedded Software Packages in STM32CubeMX (latest version v5.4.0). And if I download it, and then try to add the zip to Cube, it says it's not a supported format.

So instead I just unzip the package and look at the code, which is fine. At least it unzips the project contents, rather than a Windows-only exe like the Bluetooth packages!

Anyhow I just thought I'd share, as it might be useful for others.

SKris.1616
Associate III
March 3, 2020

Any suggestion how to use the expansion package for the same?

WFila.1
Visitor II
November 6, 2020

@SKris.1616​ , the expansion package is not what you think. The way I understand it, it is not intended to enrich the CubeMX GUI with new features adding mic usb profile or similar, it is only a handwritten example that you can take and adapt.

I tried to do the same as what is suggested in this thread, and I have to admit that it is not a trivial thing. The expansion example has a rewritten USB class middleware, so not easy to cut the middleware only, the whole example has to be ported. Also, of course CubeMX IDE does not allow to change the target, so a new example has to be re created if the target is different. Also if you do not want to run it on the exact same example board, the BSP has to be re-written and cut out of all dependencies.

What I learned from my investigation is that USB is not something like a serial port application that you can easily port, multiple API levels have to be edited depending on the needs. And especially if connection with DMA is required, then you'd have to touch the metal to do that.

I initiated a github repo where I added a flow diagram analyzing the USB stack in different examples.

My goal is similar to this thread, the first step I had as a goal when starting with an STM audio device is to create a loopback device, inject something into the STM from a host PC and then get it back, that is the basis of testing and tooling to check if what is happening in the STM is really what we intend to do. I also would like to use the black pill (STM32F411) otherwise as a fallback an STM32F407, but in both cases a custom board and not an existing discovery demo.

This is going to be long and difficult especially if I only work on this as a hobby in my free time, if someone wants to help to achieve this together, feel free to get in touch with me :

https://github.com/STM32Libs/black_pill_audio