Skip to main content
aurelien23
Associate III
October 14, 2015
Question

SPC564B74 Pin Wizard Issues in SPC5 Studio 3.6 (Pin Wizard 3.6)

Posted on October 14, 2015 at 15:30

Pin wizard was so buggy on SPC564B74L7 I decided to use the standard declaration. On SPC56EL60's RM we can find input mux select config (PSMI) for each input function. On SPC564B74 the RM the PSMI config are placed in another table which makes configuration horrible...

Concerning the pin wizard, it detects error on next opening and worst, it introduce error like declaring many times PORT_A pin 0, 1, 2... Please fix that feature.

    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    October 15, 2015
    Posted on October 15, 2015 at 17:11

    Issue solved on S¨PC5Studio 3.7.0

                    BR

                                     Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.