STm32F205RBt6 as USB Host, interfacing code for pen drive
1. Need to interface pen drive with stm32f205rbt6 for logging data in text file in pen drive.
2. Generated code from stm32cube & link for total code is here:
3. Made changes in fatfs.c file generated as below.
4. Problem is code always struk in if(FR_OK != res) & return disk_error always. What error I am doing.
5. is there any example code for STM32F2 using pen drive for storage purpose to see exactly where changes are to be made.
&sharpinclude 'fatfs.h'
uint8_t retUSBH; /* Return value for USBH */
char USBHPath[4]; /* USBH logical drive path */FATFS USBHFatFS; /* File system object for USBH logical drive */FIL USBHFile; /* File object for USBH */FRESULT res;/* USER CODE BEGIN Variables */
/* USER CODE END Variables */
void MX_FATFS_Init(void)
{ /*♯♯ FatFS: Link the USBH driver ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ retUSBH = FATFS_LinkDriver(&USBH_Driver, USBHPath);/* USER CODE BEGIN Init */
/* additional user code for init */ /* USER CODE END Init */ res = f_mount(&USBHFatFS , USBHPath ,0U); if(FR_OK != res) { while(1); } res = f_setlabel('DATA DISK'); if(FR_OK != res) { while(1); } res = f_open(&USBHFile, '/_SERIAL.txt', FA_OPEN_ALWAYS); if(FR_OK != res) { while(1); } }/**
* @brief Gets Time from RTC * @param None * @retval Time in DWORD */DWORD get_fattime(void){ /* USER CODE BEGIN get_fattime */ return 0; /* USER CODE END get_fattime */ }#usb-host #stm32f205