Skip to main content
vromanov
Associate III
March 15, 2016
Question

STM32 FOC SDK & CubeMX

  • March 15, 2016
  • 2 replies
  • 848 views
Posted on March 15, 2016 at 15:44

hi!

Can be STM32 FOC SDK & CubeMX generated code used in same project? We already have some libraries based on CubeMX. 

This topic has been closed for replies.

2 replies

Gigi
ST Employee
April 1, 2016
Posted on April 01, 2016 at 15:13

Ciao Vladimir

No, is not possible at the moment because the FOC SDK is based on the standard peripheral library and the code generated by the CubeMX is based on CubeHAL.

We plan to converge the FOC SDK versus the CubeMX but this will not be ready very soon.

Ciao

Gigi

Laurent Ca...
Senior III
June 17, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards