Skip to main content
camilomelo88
Associate
July 11, 2014
Question

GUI Library STM3241G EVAL BOARD PROBLEM

  • July 11, 2014
  • 3 replies
  • 735 views
Posted on July 12, 2014 at 00:04

Hi to all,

I'm really new with STM products, I have a discover board STM3241G-EVAL, I'm going to try to explain my problem with the GUI embedded library:

- The configuration of the source files is done, I can display icons, text, buttons in the LCD.

- I use the STM software to generate the screens for my app, but here is my problem, I wanna use icons like buttons, but if a screen have more that 3 icons, the program goes to the BusFault_Handler function.

Here is a part of my code:

This part is when the code runs fine:

GL_Page_TypeDef *CurrentScreen;

GL_Page_TypeDef inicio;

Create_PageObj( &inicio ); 

GL_PageControls_TypeDef* TEXT2= NewLabel(5,(uint8_t*)''HOLA MUNDO'',GL_HORIZONTAL,GL_FONT_SMALL,TEXT1Color);

    AddPageControlObj(303,120,TEXT2,&inicio);

       

        /*GL_PageControls_TypeDef* ImgConfig= NewIcon (1,ImgConfig_Image,30,30,GL_NULL);

    AddPageControlObj(303,176,ImgConfig,&inicio);

        */

        GL_PageControls_TypeDef* ImgTerminal= NewIcon (2,ImgTerminal_Image,30,30,GL_NULL);

    AddPageControlObj(303,64,ImgTerminal,&inicio);

        

        GL_PageControls_TypeDef* ImgSave= NewIcon (3,ImgSave_Image,30,30,GL_NULL);

    AddPageControlObj(303,16,ImgSave,&inicio);

inicio.ShowPage(&inicio,GL_TRUE);

 /***************************************/

but, if you uncomment the line that appear like comment, then, the problem happens and the BusFault appear

#stm32
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    July 11, 2014
    Posted on July 12, 2014 at 00:39

    It's not really a ''discovery'' board ST has some much lower cost/function boards with that naming.

    You might want to double check what kind of heap size you have, and if there are any other defines limiting object arrays to a couple of items
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    camilomelo88
    Associate
    July 11, 2014
    Posted on July 12, 2014 at 01:07

    thanks a lot for your quickly answer, like I said I'm new on this, Can you explain me how can I configure the heap size in IAR?

    Montassar BEN ROMDHANE_O
    Visitor II
    July 14, 2014
    Posted on July 14, 2014 at 11:49

    Hi melo.camilo,

    To edit you IAR project heap size, you've just to:

    - Go to Project

    â–º

    Options

    â–º

    Linker

    â–º

     Config Tab

    - Edit Linker configuration file

    - In the box that pops up there is a Stack/Heap Sizes tab

    - You can now edit the HEAP value.

    With regards.