Skip to main content
hariprasad
Associate III
January 19, 2015
Question

Issue while Enabling and Disabling Timer

  • January 19, 2015
  • 0 replies
  • 714 views
Posted on January 19, 2015 at 06:54

Basically what my problem is Once I de-init the Timer after a successful operation I'm not able to re-init it again...

I am writing a program to generate a delay using timer whose delay canbe varied according to the user defined value. But for the First timeI'm able to generate the desired delay but Once I de-initialize I'm notable to reinitialize the timer again

 void TIM2_irq(void)

{

    if (TIM_GetITStatus(TIM2, TIM_IT_Update) != RESET)

    {

        count++;

        TIM_ClearITPendingBit(TIM2, TIM_IT_Update);

        if(count == Max_Cnt )

        {

            flag=1;             //Once the defined count is reached set the flag

           

TIM_DeInit(TIM2); 

  //Deinitialise the Timer

        }

    }

}

void delay_using_TIM(float delay_val)

{

    Max_Cnt = delay_val *10;

    NVIC_InitTypeDef NVIC_InitStructure;

    TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

    /* Enable the TIM2 gloabal Interrupt */

    NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;

    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;

    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

    NVIC_Init(&NVIC_InitStructure);

    /* TIM2 clock enable */

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

    /* Time base configuration */

    TIM_TimeBaseStructure.TIM_Period = 5;

    TIM_TimeBaseStructure.TIM_Prescaler = 0x410;        // Verfied 100 microsec for timer expiry

    TIM_TimeBaseStructure.TIM_ClockDivision = 0;

    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

    TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);

    /* TIM IT enable */

    TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE);

    /* TIM2 enable counter */

    TIM_Cmd(TIM2, ENABLE);

    while(!flag);

    flag=0;

}

int main()

{

    while(1)

    {

        GPIO_SetBits(GPIOB, GPIO_Pin_6);    //Gpio is already initialised

        delay_js(6.2);

        GPIO_ResetBits(GPIOB, GPIO_Pin_6);

        rtos_delay_milliseconds(10);

    }

}

Is this the proper way of de-initializing the Timer ?

Please help

#stm32f4 #discovery #stm32f2 #timers
This topic has been closed for replies.