Associate II
February 10, 2015
Question
Rise time of SPI Signal
- February 10, 2015
- 1 reply
- 949 views
Posted on February 10, 2015 at 10:50
Hi
I am using STM32F103RBT6
@72MHZ I use SPI with DMA to stream data from memory to GPIO SPI Prescaler is 4 GPIO is configured as output push-pull and speed 50MHz The problem is that the data output rise and fall time is very slow, instead of getting square wave out of the scope for 0xAA data I get sine wave ''snapshot attached'' How I can get square wave with good rise and fall time at this frequency? Salam Hossam Alzmor #gpio-risetime