Question
STM32F105 SPI2 issue
Posted on March 13, 2015 at 19:06
Hello all,
I faced problems with SPI2. First I interfaced a graphic LCD on SPI bus and could not get to working properly, though it works well on an Atmel 8 bit controller. Spent more than 3 weeks without much luck. Now I interfaced Spansion flash memory. This chip supports reading manufacturer and device identification. When queried it must return 0x15. On STM32F105 returns 02, whereas 0x15 (correct value) is returned on 8 bit controller. Checked clock polarity. Here is my SPI initialization code. Any suggestions please? Thank you. GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_Init(GPIOB, &GPIO_InitStructure); SPI_InitStructure.SPI_Mode = SPI_Mode_Master; SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; SPI_InitStructure.SPI_NSS = SPI_NSS_Soft; SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; // SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_64; SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB; SPI_Init(SPI2, &SPI_InitStructure); // currently used SPI on this board SPI_Cmd(SPI2, ENABLE); #stm32f105-spi2