Skip to main content
mikemanzano.javier9
Associate III
March 30, 2016
Question

STM32F103ZE UART Tx Random Frame Error

  • March 30, 2016
  • 3 replies
  • 918 views
Posted on March 30, 2016 at 17:09

Hi,

I like to ask opinion.

Currently, in my project, I am using several UART. I connected a logic analyzer on Tx and Rx of one channel. Then in Tx, in random bytes, I saw frame error indicated by extra bit space at the end of a byte. The receiving terminal can recognize bytes with frame error however it looks dirty.

At first im operating at high baudrate, but when I lower baudrate to 9600, it still occur.

Also I thought, because the port header is near power jack but i proven it not. I use another UART channel in which its header is far from power source and the frame error still occur.

I also thought its because of sampling rate, but even if I use already 24MSample per second, frame error still occur.

In Rx, the frame error doesnt happen. only in Tx.

Any idea what went wrong?

Regards,

Mike

    This topic has been closed for replies.

    3 replies

    mikemanzano.javier9
    Associate III
    March 31, 2016
    Posted on March 31, 2016 at 09:14

    I attached screen shot of the logic analyzer capture.

    ________________

    Attachments :

    frame_error.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0rq&d=%2Fa%2F0X0000000bem%2FemZrkj5qEjxHHwexVpBwhpSjhrPnVuSIrmDySbezhWE&asPdf=false
    mikemanzano.javier9
    Associate III
    March 31, 2016
    Posted on March 31, 2016 at 09:31

    Hi,

    Im sorry.. Just now I learned the answer to my question.

    I did not notice that the machine side is sending with parity even and the application is sending without parity.

    its already resolve.

    thank you for time.

    regards,

    mj

    Walid FTITI_O
    Visitor II
    March 31, 2016
    Posted on March 31, 2016 at 11:49

    Hi javier.michael,

    Thanks for your contribution and implimenting your feedback after you finding issue.

    -Hannibal-