Question
CubeMX Feature Request
Posted on November 29, 2016 at 22:26
Hello,
I like CubeMX and would like to suggest a feature for the report generator. I use Nucleo boards a lot for development and small projects and the support for it is really great, but I always have to look up the layout of the Nucleo headers. I usually end up on mbed.org like for the F401: https://developer.mbed.org/platforms/ST-Nucleo-F401RE/ And I was wondering if that would not be a great thing to have in the report generated by CubeMX, alongside the pin layout already there. I would suggest a layout similar to the mbed website with all the available ports + special functions, and also a extra column for the own pin label. Because the basic layout is the same for the Nucleo32/64/... a general image with some custom rendered text should do the trick. Maybe the information (like pin mapping) is also already available in CubeMX. The name/type of the Nucleo Board at least is already there. I am looking forward hearing from you. Sincerely Markus #feature-request