Skip to main content
logan
Associate II
August 16, 2014
Question

USART2 baud rate coming out 1.5x slower than setting on STM32F4

  • August 16, 2014
  • 4 replies
  • 925 views
Posted on August 16, 2014 at 04:30

I'm trying to simply send a character over and over to my computer using a USB to TTL adapter and USART2 on the STM32F4 discovery board. I have USART2 configured for 9600 baud which would give 104us bit pulses.

After getting junk characters on the computer, I looked at the TX signal on my scope and saw the bit widths were about 160us, or a baud rate of ~6250 bps. In my program if I set the baud rate to 9600*1.5 I actually get 9600 baud.

All of my reading seems to suggest this is an issue with a clock setting somewhere. Most commonly I see people having an incorrect value of HSE_VALUE. My HSE_VALUE is indeed set to 8000000 for the 8MHz crystal. I also even added -DHSE_VALUE=8000000 into my CFLAGS. Here are some of my other clock settings from system_stm32f4xx.c:

PLL_M: 8

PLL_Q: 7

PLL_N: 336

PLL_P: 2

These all seemed correct to me, but I could be missing something. I'm really at a loss here for what's going on. I'm hoping someone can figure it out. Let me know if you need any additional information. Thanks!

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    August 16, 2014
    Posted on August 16, 2014 at 06:42

    Use the MCO pin (PA8) and configure it to output internal clocks, and measure those on a scope.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    logan
    loganAuthor
    Associate II
    August 16, 2014
    Posted on August 16, 2014 at 09:09

    I first added code to the program to output RCC_MCO1Source_HSE. It showed the correct 8 MHz on the scope. I then checked RCC_MCO1Source_PLLCLK on MCO1 and it was 168 MHz.

    I also looked at RCC_MCO2Source_SYSCLK with MCO2 and it was 168 MHz also.

    Any of these results seem out of the ordinary to you? Thanks.

    Tesla DeLorean
    Guru
    August 17, 2014
    Posted on August 17, 2014 at 05:11

    The maximum output for pins is about 90 MHz, so normally you'd need to divide down the 168 MHz.

    Discrepancies between measured and desired baud rates stems from a difference between the actual clock being used, and the value the software believe is being used.

    The HSE_VALUE of 25 MHz v 8 MHz typically results in a 1:3.125 distortion, not 1.5, which is more indicative of something running at 12 MHz.

    You could print out HSE_VALUE and inspect it's value in various object files.

    9600 baud should have a bit time of ~104.2 us
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    August 17, 2014
    Posted on August 17, 2014 at 05:12

    Suggest you attach a complete project for whatever tool chain you are using.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..