Skip to main content
bve
Associate
August 26, 2014
Question

Problems due to STM32F417 Silicone Revision 1?

  • August 26, 2014
  • 4 replies
  • 1036 views
Posted on August 26, 2014 at 16:44

Dear community,

one of our products uses a STM32F417IGH6 controller and has previously been build using silicone revisions A and Z. The current batch is the first with silicone revision 1 and serveral problems came up. 90% of the boards will not connect to a debugger (e.g. STLink/V2 using STLink Utility V3.4.0) and therefore cannot be programmed or tested, no matter if using SWD or JTAG. 5% are able to connect from time to time and 5% can connect reliably to the debugger. Reading these devices, I can verify, that the device is empty (0xFF on all addresses), but STLink Utility shows Revision ID: Rev. X, while the package is marked ''1''. All devices have the datecode 427.

There are no changes to PCB or other populated parts, the only change is the STM32's revision. The errata sheet has also no item, that seems to be related to debugging.

#stm32f417
This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
August 26, 2014
Posted on August 26, 2014 at 17:09

Do you have connectivity to NRST? How about the BOOTx pins?

Are you using the most current ST-LINK firmware, and Utilities? Have you tried ''Connect Under Reset'' mode? Have you tried other more commercial JTAG/SWD pods?
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
bve
bveAuthor
Associate
August 27, 2014
Posted on August 27, 2014 at 08:39

Dear Clive1,

we are using the ST-Link Utility v3.4.0 with USBDriver.dll v4.3.3.0 and the firmware in the ST-Link/V2 is V2.J21.S4. All was downloaded directly from ST's website and reinstalled, so I'm quite sure, this is the latest version.

NRST is connected to a reset controller, which works fine, verified on an oscilloscope, and is also connected to a legacy 20pin ARM debug connector. BOOT0 is pulled up and also connected to a switch to allow to pull it high or low. Both modes made no difference. BOOT1 is pulled down by a 10k resistor.

No option in the ST-Link does make a difference, ''connect under reset'' was the first thing I tried, since the utility recommended it.

Andrew Neil
Super User
August 27, 2014
Posted on August 27, 2014 at 08:52

Silicon

e

!= Silicon

http://en.wikipedia.org/wiki/Silicone

http://en.wikipedia.org/wiki/Silicon

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
bve
bveAuthor
Associate
August 27, 2014
Posted on August 27, 2014 at 09:10

Thanks for the remark, but I don't know how to change the topic titel, and I'm also quite sure all in this forum know what I ment.