Skip to main content
gilberce
Associate
September 11, 2014
Question

stm32439i-eval2 LCD usable definition ?

  • September 11, 2014
  • 2 replies
  • 686 views
Posted on September 11, 2014 at 16:38

Hi,

I was wondering why in the stm32439i-eval2 dev board, the

am640480G5TNQW  LCD is configured to be used in a 480x272 (unusual) defnition.

Is it possible to use it at 640x480 as part of driver allow it ?

Moreover, the camera embedded is a 2MP, so again why the image in the demo is cropped to the lcd definition ?

Regards

#stm32439i-eval2-am640480g5tnqw
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    September 11, 2014
    Posted on September 11, 2014 at 17:03

    Probably because most of the original STM324x9I-EVAL boards had an MB1046 panel a 16:9 480x272 display? And not the MB1063

    I've seen demo packages built for both different panels, inquire via you ST FAE or rep.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    gilberce
    gilberceAuthor
    Associate
    September 16, 2014
    Posted on September 16, 2014 at 15:35

    ty Clive,

    I got the 1063, looking for enabling a wider display.

    Btw the CAMERA to USB disk is not functionnal on the 1063. The dislay his cut on the bottom half and there are 4 minidisplay with lacking lines on the top.

    When I got time I'll look further.

    Regards.