Skip to main content
Johanan1
Associate III
October 3, 2014
Question

Bug in stm32f4xx_hal_nor.c

  • October 3, 2014
  • 1 reply
  • 398 views
Posted on October 03, 2014 at 20:20

In  HAL_NOR_GetStatus(..) timeout is not working due to an error:

-----------------

while(status != NOR_SUCCESS)

  {

    /* Get tick */

    tickstart = HAL_GetTick(); // this should be before the while !!!

    /* Check for the Timeout */

    if(Timeout != HAL_MAX_DELAY)

    {

      if((Timeout == 0)||((HAL_GetTick () - tickstart ) > Timeout)) ;// AS it is this will always be ==

      {

        status = NOR_TIMEOUT; 

      } 

    } 

.

.

.

}

-----------------------------

I have no idea who to report this, so I post it here.

Johanan

    This topic has been closed for replies.

    1 reply

    Montassar BEN ROMDHANE_O
    Visitor II
    October 7, 2014
    Posted on October 07, 2014 at 12:35

    Hi Johanan,

    We have already the limitation in the STM32Cube HAL bugs list and will be fixed in next releases of CubeF4. Thanks for the report.

    Regards,

    Heisenberg.