Skip to main content
amalpartout
Associate
March 16, 2015
Question

initializing UART2 of STM8s105 in asm coding

  • March 16, 2015
  • 1 reply
  • 1083 views
Posted on March 16, 2015 at 13:40 hello, here under my asm code for initializing UART2 of STM8s I use STVD IDE with stm8s discovery. when I put a break point at the end of the init, all the UART2 peripherals remains at 0x0000. I don't understand because I have init many others peripherals GPIO, Timer ...

;Uart variables
M EQU 4 ; 8 ou 9 bit CR1 
stop EQU 5 ; 1 stop bit CR3
bits EQU 4 ; 2 stop bit CR3
TC EQU 6 ; TC flag fin d'envoi
TXE EQU 7 ; TXE flag write data
CKEN EQU 3 ; clock mode in CR3
REN EQU 2 ; REN bit recept mode in CR2
TEN EQU 3 ; TEN bit transmit mode in CR2
; init UART2
reset_uart_register
mov UART2_CR1,#0 
mov UART2_CR2,#0 
 mov UART2_CR3,#0
init_UART2 ; 2400 bauds = 000.000 / 2200 = 6666d = 1A0B hex
bres UART2_CR1 , #M ; word lenth 8 bits
 bset UART2_CR3 , #stop ; 2 bits stops
bset UART2_CR3 , #bits ; 2 bits stops
mov UART2_BRR1 , #$A0 ; UART2 Baud Rate Register 1
mov UART2_BRR2 , #$1B ; UART2 Baud Rate Register 2
ld A , UART2_CR3
''break point'' nop
rim ;reset the cpu interupt mask 
 ; end of initialisation of all peripherals

hereunder a screenshot of the STVD IDE at the break point thanks for your help. Joël
    This topic has been closed for replies.

    1 reply

    amalpartout
    Associate
    March 16, 2015
    Posted on March 16, 2015 at 23:02

    I have found my problem .  I had remove UART clock .     grrrr !!!

     mov CLK_PCKENR1 , #%11110000 ;supprime le clock sur les oscillateurs pour les UART , SPI et I2C   /!\ 

    replace by 

     mov CLK_PCKENR1 , #%11111100 ;supprime le clock sur les oscillateurs pour les

    UART

    , SPI et I2C   /!\