Skip to main content
davide
Associate III
June 24, 2017
Question

DFU Bootloader for STM32L072xx

  • June 24, 2017
  • 1 reply
  • 897 views
Posted on June 24, 2017 at 14:53

Hi there,

I'm facing some problem in getting a STM32L072 MCU in DFU (USB) mode by jumping to the Bootloader in-code.

Following other posts suggestion and the AN2606 i've written these two functions:

#define

RESET_TO_BOOTLOADER_MAGIC_CODE      0xCAFEBABE

uint32_t

dfu_reset_to_bootloader_magic;

1) The function that I call to set a token in memory and trigger a soft-reset:

/*

 * Jump to the DFU Mode for firmware upgrade using USB

 */

void

dfuse_RunBootloader(

void

)

{

    dfu_reset_to_bootloader_magic = RESET_TO_BOOTLOADER_MAGIC_CODE;

    NVIC_SystemReset();

}

2) The function that get executed as first function in the main:

/*

 * Check if a DfuSe

Bootloader

request was triggered

 * and jump to the dedicated internal routine.

 */

void

dfuse_CheckAndRun(

void

)

{

   

if

(dfu_reset_to_bootloader_magic == RESET_TO_BOOTLOADER_MAGIC_CODE) {

        dfu_reset_to_bootloader_magic = 0;

        

// Just to be sure that's all de-initialised

        HAL_RCC_DeInit();

        HAL_DeInit();

        __HAL_REMAPMEMORY_SYSTEMFLASH();

        __ASM

volatile

(

'

movs

r3, #0\

nldr

r3, [r3, #0]\nMSR

msp

, r3\n'

: : :

'r3'

,

'

sp

'

);

       

// Application Interrupt and Reset Control :: resetting the peripherals, change the value to 0x05FA0001

        {

          

#define

SCB_AIRCR_VECTKEY_RESET (0x05FA0001)

           SCB->

AIRCR

= SCB_AIRCR_VECTKEY_RESET;

        }

        ((

void

(*)(

void

)) *((

uint32_t

*) 0x00000004))();

    }

}

After the jump, the MCU goes correctly to the System Flash Memory area containing the Bootloader but no DFU USB device appears in Windows (so nothing can be done with DfuSe). 

Did I miss something before the jump to the code / did I made some code error?

Thank you for your help and I hope this question will help also other people!

Davide

    This topic has been closed for replies.

    1 reply

    CHABIN.Laurent
    Associate II
    November 21, 2017
    Posted on November 21, 2017 at 11:20

    You can take my rather functional sample code here

    https://community.st.com/0D50X00009Xkg1sSAB