Skip to main content
ijhar09
Visitor II
Feb 6, 2015 6:36 PM UTC
Question

problem in compiling code using stsw-stm32100 library

Posted on February 06, 2015 at 19:36

hello every body,

i generated header files using MC workbench, and then copy them into sys_drive_param folder. then when i open workspace in project folder. it contains only STM32F30x_userpoeject, but according to the um1054 mannual , there should also be STM32F30x_MCLibrary,  can i compile the code without adding STM32F30x_MCLibrary, and batch build is necessary for web distribution lib.?

 please guide me..

thanks
This topic has been closed for replies.

1 reply

Gigi
ST Employee
Mar 20, 2015 3:46 PM UTC
Posted on March 20, 2015 at 16:46

Ciao

I think that is the same issue covered 

/7c38d537

.

Ciao

Gigi