Skip to main content
Andrzej Sier??ga
Associate
March 6, 2018
Question

Stm32CubeMx and Java 9

  • March 6, 2018
  • 11 replies
  • 2850 views
Posted on March 06, 2018 at 10:33

Why Stm32CubeMx doesn't work with Java 9 (9.0.4)?

I can't use Java 8 for some reason. Many other useful applications like eclipse are compatible with the newest Java version.

    This topic has been closed for replies.

    11 replies

    ST Technical Moderator
    March 12, 2018
    Posted on March 12, 2018 at 10:45

    Hello

    Sierzega.Andrzej

    ,

    Which CubeMx version are you using ?Could you please precise in details your OS environment (Linux, Windows..) ?

    May be you can try uninstallingany installed version of Java before to install the new one, as the new installation of java doesn't automatically replace the old installations.

    Best Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Andrzej Sier??ga
    Associate
    March 12, 2018
    Posted on March 12, 2018 at 11:25

    Hello Imen,

    I installed the lastest version of CubeMx. I use Windows 10.

    Using Java version 8 I have no problem with CubeMx. When I fully uninstall Java 8 and install only Java 9 I'm getting such error:

    0690X0000060A1YQAU.png

    This problem can be solved only by programmers of CubeMX by compiling it for using Java 9. This problem is known for every software developers that must support new java version.

    My version of Java is:

    0690X00000609z9QAA.png

    Regards

    Andrew

    Kuba Miszcz
    Visitor II
    April 28, 2018
    Posted on April 28, 2018 at 19:45

    I have same issue,

    system Win10 64-bit,

    `jdk-10.0.1_windows-x64_bin` installed on fresh system (so no other Javas installed),

    `SetupSTM32CubeMX-4.25.0`

    and same error message :\

    Houda GHABRI
    ST Employee
    May 7, 2018
    Posted on May 07, 2018 at 17:33

    Hi

    Sierzega.Andrzej

    ,

    STM32CubeMX doesn't support Java9 for the moment.You can use java8.

    Regards,

    Houda

    ASaba
    Associate
    November 28, 2018

    I use java8. It does not work!0690X000006CXY4QAO.jpg

    George Small
    Associate
    May 13, 2018
    Posted on May 13, 2018 at 16:52

    I also am having this issue, can not run Eclipse Oxygen.3 and 

    STM32CubeMX

     on the same Java version.  Hard Java version requires multiple Java installs, not advised.  Please address.

    October 20, 2018

    I would like to refresh this thread. Please, build the software with the newest JDK possible, currently version 10. It is very confusing, the software doesn't run and complains about missing JRE 7. It works also with JRE 8, but not with 9 nor 10.

    Thank you,

    David

    john doe
    Senior III
    November 29, 2018

    here's a better suggestion - bundle the appropriate JRE with the application, like many other developers do.

    ASaba
    Associate
    November 29, 2018

    I'm just trying to run the installation. What kind of application is it that he needs to dance with a tambourine to install it? I dont know where to search for java7. Installation redirects me to java8 page.

    After Forever
    Senior III
    November 29, 2018
    SF??r
    Associate III
    September 1, 2020

    Fails with new Win10 PC... Tests some (or all?) JRE Versions... switch over to NXP Chips and Software -> solved

    -> JRE 8 LTS -> not working (readme excludes only subversion 251)

    -> JDK 11 LTS (no JRE available) -> working

    -> newest java version -> not working