Skip to main content
stephane239955
Visitor II
July 17, 2017
Question

STM32L071 : adjust RTC prescaler when using LSI

  • July 17, 2017
  • 1 reply
  • 710 views
Posted on July 17, 2017 at 09:24

Hi, 

My projetct using RTC based on LSI : I've see a code example where the TIM21 Input Capture of TIM_CHANNEL_1 is connect internally to the LSI clock output; to mesure periode and ajust prescaler (STM32Cube_FW_L0_V1.9.0\Projects\STM32L073RZ-Nucleo\Examples\RTC\RTC_LSI)

I'm trying to migrate this example on STM32 Cube, because my project use it and I'm not alone to developp, more secure to configure low level only one time with Cube, to prevent futher modifications 

But it doesn't work, problem to remap LSI : Is there someone who have done this , is it working? How to remap LSI TIM21_TI1_LSI? 

Thanks for your help

Best regards

#lsi-rtc #rtc-calibration #stm32l0
This topic has been closed for replies.

1 reply

waclawek.jan
Super User
July 17, 2017
Posted on July 17, 2017 at 11:46

But it doesn't work,

How?

Post code. Check the read-out values from respective registers.

JW