Question
STM32F0 with HAL driver and EEPROM emulation
Posted on February 12, 2015 at 16:48
Hello,
I am curently working on an application generated by the STM32cubeMX software. This application use the folowing HAL library's: tim,adc,dma,uart,gpio... I have to implement an erase and write non volatile memory fonctionality. At first I have used the HAL_Flash lib but I can write the memory only one time. The application has to write multiple time in the memory with fixed data address.I have found the AN4061wich is very interesting. I have downloaded theSTSW-STM32117 exemple but this one doesn't use the HAL library. I can't run both HAL and non-HAL library at the same time. Is anyone got a solution wich is not to re-code all my application with the non-HAL lib? Thank's a lot!