Skip to main content
Tesla DeLorean
Guru
February 16, 2018
Question

STM32H7x3 RM0433 suggestions

  • February 16, 2018
  • 1 reply
  • 489 views
Posted on February 16, 2018 at 22:23

0690X00000604OkQAI.jpg

http://www.st.com/content/ccc/resource/technical/document/reference_manual/group0/c9/a3/76/fa/55/46/45/fa/DM00314099/files/DM00314099.pdf/jcr:content/translations/en.DM00314099.pdf

 

Here are some observations/suggestions

The document contains a number of diagram's whose text is not searchable in Adobe Acrobat Reader DC 2018.009.20050

There is a lack of coherency in the naming throughout the document, making references in one location difficult to correlate with descriptions in others, and impossible to search effectively.

Table 51 Kernel clock distribution overview

The ''Peripherals'' column on the left should have the names of the clocks as it seen everywhere else.

ie SDMMC1 should make reference to sdmmc_ker_ck naming

Figure 46 Kernel clock distribution for SDMMC, QUADSPI and FMC

SDMMCSEL, sdmmc_ker_ck do not appear searchable, come up as block characters                          when cut-n-pasted.

8.4.17 RCC Domain 1 Kernel .. (RCC_D1CCIPR)

SDMMCSEL: SDMMC kernel clock source selection

Need to explicitly name ''sdmmc_ker_ck'' here so it cross references with all other uses, like per_ck is in CKPERSEL[1:0], and is searchable/indexed

This is just one example, but is a systemic issue in the document and all other places refer to clocks, etc by their internal net names.

    This topic has been closed for replies.

    1 reply

    Nesrine M_O
    Associate
    March 30, 2018
    Posted on March 30, 2018 at 15:36

    Hi

    Turvey.Clive.002

    ,

    Thank you very much for highlighting theses document issues, they are reported internally.

    Sorry for the inconvenience it may bring.

    -Nesrine-