Skip to main content
Tesla DeLorean
Guru
September 30, 2015
Question

STM32L4 Ultra-Low-Power MCU Google Hangout Tomorrow

  • September 30, 2015
  • 11 replies
  • 1574 views
Posted on September 30, 2015 at 22:00

Not sure it was mentioned here, but just an FYI. It's done in the morning in the North American territory, so should be reachable by the European audience late afternoon.

Google Hangout ''Getting started with STM32L4, latest ST Ultra-low- Power Microcontroller'' on Thursday, October 1st at 9 a.m. PDT.

https://plus.google.com/u/0/events/cpjc6185invhkcbbgflbfv2uhkc

Not sure if it's going to be much more than a slide deck, but they normally do a Q&A so if you have pressing questions this would be a good opportunity to get mind share with those in the sales and marketing, and the FAE's

The day long seminar series kicks off 20-Oct-2015 in Chicago

#lets-break-the-internets
    This topic has been closed for replies.

    11 replies

    gregstm
    Senior II
    October 1, 2015
    Posted on October 01, 2015 at 14:35

    Sounds interesting. Unfortunately a bit late here in Australia (1:30am). If someone could pin them down about details of an LQFP48 package version  it would be appreciated.

    AvaTar
    Senior III
    October 1, 2015
    Posted on October 01, 2015 at 15:16

    > Google Hangout ''Getting started with STM32L4, latest ST Ultra-low- Power Microcontroller'' on Thursday, October 1st at 9 a.m. PDT.

     

    That is about 5:00 CET (central european time) - so says the reminder mail from ST.

    Amel NASRI
    ST Technical Moderator
    October 1, 2015
    Posted on October 01, 2015 at 18:13

    And this is the link to the page where you may find details on the seminars agenda: http://www.st.com/web/en/en./seminar/stm32l4-ultra-low-power-mcu-hands-on-seminar.

    -Mayla-

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    Tesla DeLorean
    Guru
    October 1, 2015
    Posted on October 01, 2015 at 18:21

    If someone could pin them down about details of an LQFP48 package version  it would be appreciated.

    Somewhat evasive of a roadmap/timeline, inferred something would appear in 2016

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    October 1, 2015
    Posted on October 01, 2015 at 19:03

    The LQFP48 question got a couple of +1's from others, the part's crying out for this kind of form-factor, not everyone needs lots of pins. Instead of non-committal answers, try and address the technical reasons why it's not already available, is the die too big, I can't believe the package is a problem like it would be for more exotic/specialized BGA ones. LQFP's are things people want to use in low cost, low complexity board designs, they are easy to manufacture in lots of markets.

    The thing that got the most hits was the question about the LL (Low Level) library, vs why can't we get the SPL. I think there's significant frustration with the abandonment of the SPL.

    Got a couple of Eclipse and Visual Studio questions, I've used the Atmel Studio guys, and it's a painfully slow running platform.

    Will it run ucLinux, I'd guess you'd ask

    http://www.emcraft.com/

    I just scratch my head about why you'd want to do this on a slow platform, what does bringing Linux to the party solve? The F7 at least has good/large external memory option, memory management and caches. Can someone given me a cogent use case here?

    http://www.st.com/st-web-ui/static/active/en/resource/sales_and_marketing/promotional_material/flyer/flstm32l4.pdf

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    waclawek.jan
    Super User
    October 1, 2015
    Posted on October 01, 2015 at 19:22

    > The LQFP48 question

    https://youtu.be/myx_UKe0SSU?t=4618

    > The thing that got the most hits was the question about the LL (Low Level) library, vs why

    > can't we get the SPL. I think there's significant frustration with the abandonment of the SPL.

    https://youtu.be/myx_UKe0SSU?t=4255

    The whole thing was pretty boring, the bulk of it was basic glossy-paper-stuff reading. I'd love to see better information-to-time ratio, should this be repeated. I hope the live seminars supply more substantial information, most of the attendees should be able to read.

    JW

    http://www.st.com/st-web-ui/static/active/en/resource/sales_and_marketing/promotional_material/flyer/flstm32l4.pdf

    gregstm
    Senior II
    October 1, 2015
    Posted on October 02, 2015 at 01:21

    Thanks for your efforts Clive and JW.

    I'm not sure why ST is so secretive about this issue (LQFP48). 

    I reckon an LQFP48 part would do more to introduce this chip to new people and new products  than any number of Discovery boards.

    My concern is that there are no technical reasons why it could not be done now - and that it is just a marketing decision. Until I see some written confirmation I will keep pestering... I mean lobbying.

    Tesla DeLorean
    Guru
    October 2, 2015
    Posted on October 02, 2015 at 03:22

    While I think the wafer scale parts might have large volumes, the number of customers is very low, whereas I think the appeal of the small LQFP is much broader. There are lots of things that are compute heavy that don't need a lot of pins.

    I'd be interested in the percentage spread for the different F4 foot prints currently.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    ST Employee
    October 3, 2015
    Posted on October 03, 2015 at 14:41

    Hello,

    Thanks for your feedbacks. Regarding the packages. Most of packages available on STM32L4 are already LQFP (LQFP64, LQFP100 and LQFP144).

    The reason to not have LQFP48 available now is not maketing but technical. Indeed it is not possible to address with the same die a very large spread of pinout for LQFP. We already adress a large range from 64 to 144 pins. 

    It will come with future derivatives. Stay tuned. :)

    Hope it clarifies.

    Thanks,

    Bertrand

    http://www.st.com/st-web-ui/static/active/en/resource/sales_and_marketing/promotional_material/flyer/flstm32l4.pdf

    gregstm
    Senior II
    October 4, 2015
    Posted on October 04, 2015 at 15:21

    Yes, that does clarify things. Thanks.